From RTSC-Pedia
revision tip
LANDSCAPE orientation[printable version] [offline version] | offline version generated on 25-Jun-2010 20:06 UTC |
C - create
Allocate and initialize a new instance object and return its handle
Contents |
Synopsis
| #include <«pkg»/«Mod».h> «Mod»_Handle «Mod»_create( [«required_args»,] const «Mod»_Params *params, Error_Block *eb ); |
Description
The create method is used to create a new instance object managed by the module.
See also
C - Instance_init | Module's instance initialization function |
[printable version] [offline version] | offline version generated on 25-Jun-2010 20:06 UTC |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved