1 /*
2 * Copyright (c) 2008 Texas Instruments. All rights reserved.
3 * This program and the accompanying materials are made available under the
4 * terms of the Eclipse Public License v1.0 and Eclipse Distribution License
5 * v. 1.0 which accompanies this distribution. The Eclipse Public License is
6 * available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
7 * Distribution License is available at
8 * http://www.eclipse.org/org/documents/edl-v10.php.
9 *
10 * Contributors:
11 * Texas Instruments - initial implementation
12 * */
13 /*
14 * ======== Timestamp.xdc ========
15 */
16
17 package xdc.runtime;
18
19 /*!
20 * ======== Timestamp ========
21 * Timestamp services
22 *
23 * This module provides `{@link xdc.runtime.ITimestampClient}` APIs for
24 * the xdc Runtime Support Library. Calls to these APIs are forwarded
25 * to a platform specific `{@link xdc.runtime.ITimestampProvider}`
26 * implementation.
27 *
28 * A user can attach their own ITimestampProvider module
29 * using the following config file command:
30 * @p(code) 31 *
32 * xdc.runtime.Timestamp.SupportProxy = xdc.useModule("usersTimestampProvider");
33 * @p 34 * If no such `{@link #SupportProxy SupportProxy}` initialization is done,
35 * the `{@link xdc.runtime.TimestampNull}` ITimestampProvider implementation,
36 * which provides null stubs for the APIs, will be attached by default.
37 *
38 * If the user is developing code using CCS, the
39 * `{@link xdc.runtime.TimestampStd}`
40 * ITimestampProvider implementation, which uses the ANSI C clock()
41 * function, may provide a satisfactory timestamp source (remember to
42 * enable the profile clock in CCS).
43 *
44 * To use the TimestampStd implementation, add the following to
45 * your config script:
46 * @p(code) 47 *
48 * xdc.runtime.Timestamp.SupportProxy = xdc.useModule("xdc.runtime.TimestampStd");
49 * @p 50 */
51 module Timestamp inherits ITimestampClient {
52
53 /*!
54 * ======== SupportProxy ========
55 * User supplied time stamp provider module.
56 *
57 * The SupportProxy module provides application/platform
58 * specific implementations of the
59 * `{@link xdc.runtime.ITimestampProvider}` APIs.
60 *
61 * If not explicitly supplied by the user, this proxy defaults to
62 * `{@link xdc.runtime.TimestampNull}`,
63 * which provides null stubs for all of the ITimestampProvider APIs.
64 */
65 proxy SupportProxy inherits ITimestampProvider;
66 }
67 /*
68 * @(#) xdc.runtime; 2, 1, 0,282; 6-23-2010 14:03:17; /db/ztree/library/trees/xdc/xdc-v41x/src/packages/
69 */
70