From RTSC-Pedia
![]() | [printable version] [offline version] | offline version generated on 27-May-2010 18:05 UTC |
XDCspec Language Summary
XDCspec language quick reference
NOTE: This document will be retired shortly, after its contents has been merged into the XDCspec Language Reference.
XDCspec is a special-purpose language for expressing the logical structure of software content in terms of three higher-level constructs -- modules, interfaces, and packages. Enforcing a clean separation between software specification and software implementation, an XDCspec source file effectively serves as a programmatic contract between content suppliers (producers) and their clients (consumers). Incorporating familiar C constructs for defining client-visible constants, types, and functions, a specification expressed in XDCspec often resembles a "cleaned-up" rendition of a legacy header file.
While comparable to an IDL (Interface Definition Language), the true power of XDCspec lies in its ability to forge a single specification that serves two congruent programming domains: [1] a target-domain, where the specified content is implemented in C/C++ and executes on a suitable hardware platform; and [2] a meta-domain, where this same content is potentially configured to match specific system requirements before target execution begins. In support of the latter, XDCspec works hand-in-hand with XDCscript -- a general-purpose language based on industry-standard JavaScript -- used by producers and consumers alike to implement host-based meta-programs that ultimately beget target executables.
Contents |
lexical-elements
The lexical structure of XDCspec closely tracks that of JavaScript, which in turn is patterned after familiar conventions originating in C. The following table summarizes the different sorts of lexical elements potentially found in an XDCspec source file:
Element | Examples |
---|---|
whitespace | space, tab, newline |
single-line comment | // text |
block comment | /* text */ |
C-style identifier | main , int32 , _private |
JavaScript number | 123 , 0xff , 6.02e23 |
JavaScript string | "hello\n" , 'abc' |
syntactic-elements
The following table summarizes the different sorts of syntactic elements appearing throughout the XDCspec reference grammar:
Element | Examples |
---|---|
syntactic production | requires-statement , unit-category |
language keyword | package , module |
language identifier | dirname , UnitName |
literal value | number , string |
literal symbol | [ , } , ; |
documentation comment | //! @xdoc |
optional term | grammar-term ? |
alternative terms | grammar-term |
zero-or-more occurrences | grammar-term * |
one-or-more occurrences | grammar-term + |
group-of terms | [ grammar-term grammar-term ] |
package-specification
Within the realm of XDCspec, a package is a programmatic element that logically contains modules and interfaces -- collectively termed units -- within its scope. Besides introducing its own public name, a package specification may identify other named packages upon which the current package in some way depends. The specification may also declare its (in)compatibility with earlier versions of the same package, as well as further constrain the level of compatibility required of any dependent packages. Specially-formatted comments embedded in package-specification source file are processed by the xdoc utility when generating HTML documentation for a set of packages.
- package-specification
requires-statement* //! @xdoc package qualified-package-name compatibility-key? { unit-declaration-list* }[;]? //! @xdoc
- requires-statement
requires qualified-package-name compatibility-key? ;
- qualified-package-name
dirname [.dirname]*
- compatibility-key
[ number [,number]* ]
- unit-declaration-list
unit-category UnitName [,UnitName]* ;
- unit-category
module | interface
- A qualified-package-name should in general be globally-unique. Packages are located in a directory with a matching name found along the system package path.
- A package-specification resides in a distinguished source file named package.xdc, found in the corresponding package directory.
- Each unit-declaration-list introduces individual modules and interfaces within the scope of the current package, all of which must be uniquely named. Units with the same name may only appear in different packages.
- Each requires-statement designates another package upon which the current package in someway depends. The requires-relation among packages cannot contain cycles.
- A compatibility-key is generally interpreted as an numeric array of the form [m,s,r,p] where m denotes major functionality, s denotes source level, r denotes specification radius, and p denotes a particular patch. A new release of a package is source-compatible with any predecessor in which m is the same, and is binary-compatible with that predecessor if s is the same as well.
- By convention, package names are composed of lowercase identifiers whereas units (modules or interfaces) are named with TitleCase identifiers.
unit-specification
A unit specification defines all client-visible programmatic features of a module or interface. While virtually identical vis-à -vis their XDCspec syntax, semantically this pair of programmatic elements are almost opposites: a module is concrete and closed, comprising a public specification accompanied by a conforming implementation; an interface is abstract and open, comprising only a public specification which others may import and ultimately implement. In general, the specification of a module or interface can inherit features from exactly one other (interface) specification, which itself can inherit additional features in the same manner -- as if the latter’s cumulative set of features had been directly defined with the unit specification of its inheritor.
The features defined within the scope of a unit partition themselves into two main groups: module-wide features, which are associated with a solitary programmatic object encapsulating the implementation of some concrete module; and per-instance features, which are associated with a family of programmatic objects individually created and manipulated by the same underlying module. Aside from auxiliary definitions of supporting constants and types (deemed module-wide for convenience), features with a meaningful run-time presence in the underlying implementation -- assignable configuration parameters along with callable functions -- can participate in either category. As with packages, special documentation comments can be associated with the module/interface as a whole as well as with any named feature defined within its scope.
In the general case, a single unit specification for a module or interface defines a presence in two congruent programming domains: [1] the target-domain, where specified features become accessible within executable programs (written in C/C++) running on some particular platform; and [2] the meta-domain, where specified features become accessible within hosted scripts (written in XDCscript) used to configure these very same target programs ahead of their execution. In some cases, the specification of a particular module or interface can be restricted to the meta-domain -- useful when constructing configuration "facades" atop legacy content as well as when distributing host-based meta-content for use in a broader range of scripting contexts.
- unit-specification
//! @xdoc metaonly? unit-category UnitNameinherited-interface?{ module-wide-feature* [ instance:per-instance-feature*]? }[;]? //! @xdoc
- inherited-interface
inherits qualified-unit-name
- qualified-unit-name
[qualified-package-name .]? UnitName
- module-wide-feature
//! @xdoc [auxiliary-definition | config-parameter | function-declaration]
- per-instance-feature
//! @xdoc [config-parameter | function-declaration]
- A qualified-unit-name effectively extends the (already) globally-unique name of the unit’s containing package. If the qualified-package-name prefix is absent, the current package name is presumed.
- A unit-specification resides in a source file named UnitName.xdc, found in the directory of its containing package.
- Each module-wide-feature or per-instance-feature introduces an individual feature with the scope of the current unit, all of which must be uniquely named. Features with the same name may only appear in different units.
- An inherited-interface designates a single interface whose features are introduced within the scope of the current unit. Any module or interface can optionally inherit features from another interface, so long as the inherits-relation among all units remains acyclic.
- Each unit manifests itself in both the target- and meta-programming domains, unless designated metaonly. As a rule, inheritors of metaonly interfaces must themselves be metaonly modules or interfaces.
auxiliary-definition
An XDCspec auxiliary definition defines a (module-wide) constant or type, often supporting other module-wide or per-instance features defined in the same unit. These definitions are also used by clients who consume this unit, both within any modules or interfaces they may specify as well as within any target (or meta) content they may implement. For the most part, the syntax and semantics of each form of auxiliary definition is patterned after a familiar programmatic construct already found in C. Further semantic restrictions guarantee auxiliary definitions have a meaningful manifestation in the meta-domain as well as in the target-domain.
- auxiliary-definition
const | enum | extern | struct
- const
const typed-declaration = initializer ;
- enum
enum EnumName { enum-value //! @xdoc [enum-value ]* //! @xdoc } [;]?
- enum-value
ENUMVAL_NAME [= initializer]?
- extern
extern typed-declaration = symbolName ;
- struct
struct StructName { struct-field* } [;]?
- struct-field
typed-declaration ; //! @xdoc
- typedef
typedef typed-declaration ;
- A const is restricted to numeric types, either standard or else enumerated. Its persistent value is defined by a statically-evaluated initializer consistent with its typed-declaration.
- An enum is a new numeric type that ranges over a finite set of named values. As in C, integer values beginning with 0 are assigned to each successive enum-value (unless altered by an explicit numeric initializer). Each named value is actually resident in the scope of the containing module or interface, and hence must be unique among all features defined in this unit.
- An extern is a special form of constant that effectively aliases an external program symbol naming a C-language function or variable. Its typed-declaration is restricted to standard C types, including arbitrary pointer-types.
- A struct defines a new aggregate type comprising a set of assignable fields of any type. Each struct-field must be uniquely named within the scope of the enclosing struct.
- A typedef effectively defines a synonym for the type specified in its typed-declaration, rather than a new type per se. As in C, typedef names can appear in other typed declarations not unlike previously-defined enum or struct names.
- By convention: UPPER_CASE identifiers are used to name a const, enum value, or extern; TitleCase identifiers are used to name an enum/struct types as well as in typedefs; and camelCase identifiers are used to name struct fields.
config-parameter
A configuration parameter is a feature that behaves like a "property" of the underlying module or instance object -- a readable (and sometimes writeable) variable of virtually any type. In the most general case, module-wide configuration parameters are assigned within the meta-domain and then become persistent constants within the target-domain; per-instance configuration parameters are likewise assignable within the meta-domain, but are limited to supporting run-time instance creation within the target-domain. Where appropriate, configuration parameters can be restricted to the meta-domain as well as designated readonly after initialization.
A configuration parameter inherited from some previously specified interface can itself be overridden -- typically to (re-)define its initial value. A configuration parameter can also be finalized, effectively freezing its definition and precluding further overrides.
- config-parameter
config-modifiers config typed-declaration [ = initializer]? ;
- config-modifiers
final? override? readonly? metaonly?
- The optional initializer must yield a value consistent with the typed-declaration, using the rules of assignment-compatibility defined by XDCscript for the meta-domain. If no initializer is supplied, the configuration parameter starts out undefined in the meta-domain.
- If override is specified among the config-modifiers for a configuration parameter, its typed-declaration as well as its use of readonly and metaonly must exactly match that of the inherited configuration parameter being overridden. Configuration parameters marked final cannot be overridden.
- A readonly configuration parameter without an initializer can still be assigned a persistent value in the meta-domain, during construction of an underlying module/instance object.
- By convention, configuration parameters names are camelCase identifiers.
function-declaration
An XDCspec function declaration generally stipulates the signature -- argument and return types -- of a callable routine implemented through a concrete module in either the target-domain or else (if so indicated) in the meta-domain; a target function also manifests itself in the meta-domain as an extern symbol of a function-pointer type derived from the stipulated signature. Following C++, default values can be specified for the last k arguments of an n-ary function, enabling the same routine to be called with as few as n-k inputs; an untyped sequence of optional trailing arguments can be also specified using the familiar ... notation. For those meta-domain functions wishing to adopt a more "weakly-typed" style supported (but not necessarily encouraged!) by the XDCscript language, their corresponding declaration in XDCspec can just contain the names for each argument.
Like configuration parameters, a function declaration inherited from a previously-specified interface can be overridden -- typically, to alter or extend the set of default argument values or else to allow optional trailing arguments. Note, though, that since interfaces are entirely abstract (void of any "default" implementation), inheritance of functions is limited to their client-visible specification; ultimately, it is concrete modules (or their delegates) that bear responsibility for implementing all functions directly or indirectly declared in their specification. With XDCspec support for Design-By-Contract forthcoming, overriding inherited function declarations becomes an essential technique for weakening pre-conditions and strengthening post-conditions specified previously through executable expressions.
- function-declaration
typed-function-declaration | untyped-function-declaration
- typed-function-declaration
function-modifiers typed-declaration ( typed-arguments? [, ...]? );
- function-modifier
final? override? metaonly?
- typed-arguments
arg-declaration [,arg-declaration]*
- arg-declaration
typed-declaration [= initializer]?
- untyped-function-declaration
function fxnName( untyped-arguments? );
- untyped-arguments
argName [,argName]*
- If override is specified among the function-modifiers for a function, its name and type signature as well as its use of metaonly must exactly match that of the inherited declaration being overridden. Functions marked final cannot be overridden.
- The optional initializer within an arg-declaration must yield a value consistent with the typed-declaration, using the rules of assignment-compatibility defined by XDCscript for the meta-domain.
- All argument names -- whether typed-arguments or untyped-arguments -- must be uniquely named on a per-function basis.
- An untyped-function-declaration is implicitly modified final and metaonly.
- By convention, function and argument names are camelCase identifiers.
typed-declaration
Generic declarations of typed identifiers patterned after the familiar (and sometimes awkward) syntax of C lie at the heart of virtually all XDCspec feature definitions. These declarations stipulate a type name, either built-in or previously-defined, followed by what is conventionally termed a declarator -- the name of the feature per se, optionally adorned with other syntactic elements. As in C, use of the *, [], and () operators within the declarator denotes new types such pointer-to(t), array-of(t), and function-returning(t)for some base type t; extra parentheses are typically used to bind the lower-precedent * operator to the declared name, especially when defining types of form pointer-to(function-returning(t)).
Beyond these familiar C constructs lifted from the target-domain -- each given a corresponding meaning in the meta-domain -- XDCspec introduces additional base types as well as more specialized forms of the array:
- the built-in type any, which subsumes all other types in the meta-domain;
- the keywords Module, Instance or Handle, signifying an opaque type referencing a concrete module, meta-domain instance object, or target-domain instance object, whose visible features are limited to those specified in the corresponding named unit;
- the keyword length in conjunction with the [] operator, signifying the type vector-of(t) whose length can be altered in the meta-domain and retrieved in the target-domain; and
- the keyword string in conjunction with the [] operator, signifying the type map-into(t) that effectively overlays direct access via string-valued keys on an underlying vector-of(t).
[Note that only a subset of the elementary C types are recognized at this time. More comprehensive support for target-domain types -- including a set of "portable" numeric types -- is forthcoming.]
- typed-declaration
[ standard-type | defined-type ] declarator
- standard-type
any | bool | float | int | string | void
- defined-type
[qualified-unit-name .]? defined-type-name
- defined-type-name
EnumName | StructName | TypedefName | Instance | Handle | Module
- declarator
declared-name ? | * declarator | declarator [ [number | length | string]? ] | declarator ( argument-types ? [...]? ) | ( declarator )
- declared-name
CONST_NAME | EXTERN_NAME | TypedefName | argName | configName | fieldName | fxnName
- argument-types
typed-declaration [,typed-declaration ]*
- The following table summarizes the meaning of certain standard-type(s) in each domain:
Type | Target Domain | Meta Domain |
---|---|---|
bool | standard C bool | standard JavaScript boolean |
float | standard C float | standard JavaScript number |
int | standard C int | standard JavaScript number |
string | standard C char* | standard JavaScript string |
- The standard-type void, as in the C-based target-domain, is basically limited to specifying the type of functions returning "no" value in the meta-domain as well. The type void* likewise preserves the semantics of a "universal pointer" in the meta-domain, assignable any value of type pointer-to(t).
- The standard-type any is only defined for the meta-domain.
- A defined-type identifies a previously defined type, either in the module or interface designated by a valid qualified-unit-name or else in the current unit.
- The declared-name at the heart of a declarator is only optional within arguments-types, typically used when declaring a type pointer-to(function-returning(t)). C reference grammars usually refer to this syntactic construct as an abstract-declarator.
initializer
An initializer is an expression that denotes either a scalar or aggregate value, and whose elementary terms are manifest constants of known types. While certainly C-like in form and substance, XDCspec scalar initializers are in fact statically-evaluated using JavaScript semantics (upon which XDCscript is based). Building on this foundation, XDCspec aggregate initializers adopt standard JavaScript notation for denoting object and array values.
- initializer
scalar-initializer | array-initializer | struct-initializer
- scalar-initializer
literal | defined-constant | unary-op scalar-initializer | scalar-initializer binary-op scalar-initializer | scalar-initializer ? scalar-initializer : scalar-initializer |(scalar initializer)
- literal
number | string | true | false | null | undefined
- defined-constant
[qualified-unit-name .]? defined-constant-name
- defined-constant-name
CONST_NAME | ENUMVAL_NAME
- unary-op
*|-|~|!
- binary-op
+|-|*|/|%|<<|>>|==|!=|<|<=|>|>=|&|||^
- array-initializer
[ ] | [ initializer [,initializer]* [,]?]
- struct-initializer
{ } | { field-initializer [,field-initializer]* [,]?}
- field-initializer
fieldName : initializer
- A literal number or string must conform to standard JavaScript, which also tracks standard C in this regard.
- A defined-constant identifies a previously defined constant, either in the module or interface designated by a valid qualified-unit-name or else in the current unit.
- The meaning and precedence of each unary-op and binary-op conforms to standard JavaScript, which likewise mirrors C. Note that JavaScript often overloads operators like + and < to accept strings as well as numbers.
//! @xdoc
Special comments embedded within a specification source file are processed by the xdoc utility when generating HTML documentation for a set of packages. These documentation comments are identified by an extra leading "bang" character -- //! for single-line comments, /*! for the block variety -- and can be juxtaposed with most named elements in the specification. Whenever multiple comments of either variety are associated with an individual specification element, their bodies are effectively concatenated into a single documentation block comprising one or more lines of text.
Markup of the form @tag, when present at the beginning of a line, further punctuates a documentation block into distinct sections comprising various styles of paragraphs. To avoid clutter in the source file due to excessive markup, most commentary can be written as "plain text" that follows some simple conventions to indicate (say) change-of-font or end-of-paragraph. Each documentation block generally comprises: [1] an untagged summary section, which is typically a "one-liner"; [2] an optional untagged details section, which may contain multiple paragraphs with additional information; and [3] a series of tagged sections, which further compartmentalize information about the associated specification element.
- //! @xdoc
summary-section details-section? tagged-section*
- summary-section
comment-paragraph
- details-section
comment-paragraph+
- tagged-section
@sectTag(ident) comment-paragraph+
- comment-paragraph
[@p[(style)]?]? textLines*
- The @a(sectName) and @b(sectName) tags create named sections that will respectively appear after or before the details section for this documentation block.
- The @c(childName) tag is used in struct, enum, or function-declaration documentation to respectively comment on one of its named children -- fields, values, or arguments. All such comments are output together as a definition list in a special section.
- The tags @field, @value, @arg, and @param are available as (more mnemonic) alternatives to the @c tag.
- An struct-field or enum-value can be immediately followed by a documentation comment, which must begin on the same line. The body of this comment is limited to a summary section.
- The @p(style) tag is used to change the prevailing paragraph style, which remains in effect until the next tag. Without any parameter, @p reverts to the default "plain-text" style in effect at the beginning of the block. The following table summarizes the different styles supported through this tag, and the interpretation each imposes on subsequent lines of text:
Style | Interpretation Of Subsequent Text |
blist | a bulleted list, with leading dashes indicating successive list elements |
code | monospace text in which whitespace is preserved |
dlist | a definition list, with leading dashes indicating successive terms; unmarked lines are the definitions |
html | text containing standard HTML markup |
nlist | a numbered list, with leading dashes indicating successive list elements |
text | "plain-text" with minimal in-line formatting; the default |
- Except for code and html, all @p styles support the following formatting conventions within the lines of text under their control:
Convention | Resulting Format |
---|---|
text | render this text in monospace |
*text* | render this text with emphasis |
blank-line | skip a line and start a new paragraph |