From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 27-May-2010 18:05 UTC | ![]() |
XDCspec - @XmlDtd
This structure can be serialized as XML
This attribute is applicable to structures only. The meta-domain representation of structures with his attribute have a function named $xml() attached to them. This function returns an E4X XML representation of the object which can be used to easily serialize this structure within XML files.
![]() | [printable version] [offline version] | offline version generated on 27-May-2010 18:05 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved