From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 27-May-2010 18:05 UTC | ![]() |
XDCspec - @Macro
This function is a macro
This attribute is applicable only to functions. If a function is declared in a spec file with "@Macro" preceding the function declaration, the generated header file will not contain a declaration for that function. The package producer must create Mod__prologue.h and Mod__epilogue.h custom header files, and define the function as a macro or a static inline function.
The package producer must use fully qualified function and parameter names in custom header files. For example, the declaration of a function in Mod.xdc in package pkgA
| @Macro Int max(Int a, Int b); |
must be accompanied with the definition that uses fully qualified names of the function
| #define pkgA_Mod_max(a, b) ((a) > (b) ? (a) : (b)) |
![]() | [printable version] [offline version] | offline version generated on 27-May-2010 18:05 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved