From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 27-May-2010 18:05 UTC | ![]() |
XDCspec - @InstanceFinalize
This module's instances require finalization
This attribute is applicable only to modules with instances. If this attribute is specified for a module, its internal instance finalize function (Mod_Instance_finalize) is called when the instance is deleted, destructed, or if the instance initializer returns an error (see @InstanceInitError ). The finalize method is passed two input parameters:
- the pointer to the instance object being deleted, and
- an integer status value; if @InstanceInitError is also specified, this status is either the return value from Mod_Instance_init or 0, otherwise this status value is not initialized.
The fragments below illustrates the instance finalize method signature for a module named Foo both with and without the @InstanceInitError attribute.
with @InstanceInitError | |
| #include "package/internal/Foo.xdc.h" /* state is the return value of Foo_Instance_init() */ Void Foo_Instance_finalize(Foo_Object *obj, Int state) { /* use state to know what needs to be finalized */ : } |
without @InstanceInitError | |
| #include "package/internal/Foo.xdc.h" Void Foo_Instance_finalize(Foo_Object *obj) { : } |
![]() | [printable version] [offline version] | offline version generated on 27-May-2010 18:05 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved