From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 27-May-2010 18:05 UTC | ![]() |
XDCscript - xdc.module
Return specified module or interface object
Contents |
Synopsis
| var moduleOrInterfaceObj = xdc.module(moduleOrInterfaceName); |
Parameters
- moduleOrInterfaceName
- the fully qualified module name of the module or interface to be loaded; e.g., "xdc.runtime.Memory" or "xdc.runtime.IHeap".
Description
xdc.module() loads the specified module or interface and returns .
Examples
To get the module object associated with the xdc.runtime.Log, the following statement should be added to the
| var Log = xdc.module("xdc.runtime.Log"); |
Return Value
xdc.useModule() returns a module object or throws an exception if
- the package containing the module or interface can not be found, or
- the module or interface is not in the specified package.
Throws
This method may throw an xdc.services.global.XDCException exception with one of the following ids:
- "xdc.PACKAGE_NOT_FOUND" - in the event that the specified package can not be found or its IDL files have not been compiled.
- "xdc.MODULE_NOT_FOUND" - in the event that the module can not be found in the specified package.
![]() | [printable version] [offline version] | offline version generated on 27-May-2010 18:05 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved