From RTSC-Pedia
revision tip
LANDSCAPE orientation[printable version] [offline version] | offline version generated on 27-May-2010 18:05 UTC |
XDCscript - Module-Body.module$meta$init
Initialize meta-domain module state
Synopsis
| function module$meta$init() |
Description
module$meta$init() is called right before the package's init() function, so its purpose is similar, but module specific initialization should be placed here.
See also
XDCscript - Module-Body.module$static$init | Initialize module's State object |
Creating Configurable Content | How to leverage the configuration process |
[printable version] [offline version] | offline version generated on 27-May-2010 18:05 UTC |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved