From RTSC-Pedia
![]() | [printable version] [offline version] | offline version generated on 27-May-2010 18:05 UTC | ![]() ![]() |
Demo of the RTSC Platform Wizard in CCSv4
Using CCStudio v4 to create a custom RTSC platform
RTSC Platform Wizard Demo Part 1: The following Flash demo shows how to use the RTSC platform wizard in CCSv4 to create a custom RTSC platform package.
When the demo pauses, click "Next" to continue. A table of contents at the end lets you review specific actions. If you don't see the demos, you can download the Flash player, or save the demo to disk.
RTSC Platform Wizard Demo Part 2: Next, you can continue to the second demo in this series shows how to further customize the memory sections defined for a platform package. It also shows how to reopen and rebuild a platform package you have created.
RTSC Platform Wizard Demo Part 3: The third demo in this series shows the files in a custom RTSC platform package and the zip file you can use to distribute the package.
See also
Demo of Customizing Memory Sections | Editing a platform package and defining your own memory sections |
Demo Showing Files in a Custom Plaform Package | Platform package directory contains zip file for distribution |
Demo Building with Custom Platform Package | Set RTSC configuration project properties and compare a platform to a generated map file |
RTSC+CCStudio v4 QuickStart | Using CCStudio v4 to create, build, and debug RTSC projects |
RTSC+Eclipse FAQs | Using RTSC with Eclipse-Based Tools |
XGCONF User's Guide | Using the RTSC Graphical Configuration Tool in CCSv4 |
![]() | [printable version] [offline version] | offline version generated on 27-May-2010 18:05 UTC | ![]() ![]() |