From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 27-May-2010 18:05 UTC | ![]() |
C - Handle downCast
conditionally move one level down the inheritance hierarchy
Contents |
Synopsis
| #include <«pkg»/«Mod».h> «Mod»_Handle «Mod»_Handle_downCast(«IMod»_Handle handle); |
Description
This function is automatically defined for all target modules that support instances and inherit from an interface, where «Mod» is the name of some module and «IMod» is the name of some interface. This function converts an abstract interface handle to an instance handle managed by the concrete module «Mod». If handle does not actually reference an instance managed by «Mod», «Mod»_Handle_downCast() returns NULL.
See also
C - Handle_upCast | unconditionally move one level up the inheritance hierarchy |
xdc.runtime.HeapMin.Handle_downCast | Client documentation for xdc.runtime.HeapMin.Handle_downCast |
![]() | [printable version] [offline version] | offline version generated on 27-May-2010 18:05 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved