1 /*!
2 * ======== Registry ========
3 * Register modules that are not statically configured
4 *
5 * This module provides a mechanism by which legacy C code can have its own
6 * module logging support, including having a name and its own diags mask.
7 *
8 * Without the Registry, all logging done by legacy C code is handled by the
9 * xdc.runtime.Main module. This means that all log events will be marked as
10 * coming from "xdc.runtime.Main", and there is only a single diags mask for
11 * controlling logging across all legacy C code. The Registry module addresses
12 * this and allows legacy C code to have the same granular control over
13 * logging as statically defined RTSC modules.
14 *
15 * To use the Registry, legacy code must define the symbol `Registry_CURDESC`
16 * to be the name of an externally declared `Registery_Desc` structure.
17 * This symbol must be defined before the inclusion of any xdc/runtime header
18 * files. If any xdc/runtime header files are included before the definition
19 * of this symbol, the Registry may not function properly.
20 *
21 * Note: by defining this symbol on the compile line, rather than in the
22 * file, one can easily compile code to be used in one of two environments:
23 * 1. a fixed configuration environment where moudles are registered
24 * via Registry_addModule(), or
25 *
26 * 2. a "normal" configurable environment in which this code is
27 * assumed to be part of the xdc.runtime.Main module.
28 *
29 * The `Registry_Desc` structure must then register by calling the
30 * '{@link #addModule}' API. The structure is typically registered and
31 * initialized within `main()`.
32 *
33 * For example:
34 *
35 * @p(code) 36 * //Define the required symbol, Registry_CURDESC, to this file's
37 * //Registry_Desc object
38 * #define Registry_CURDESC main_desc
39 * #include <xdc/runtime/Registry.h>
40 *
41 * //Declare the Registry_Desc object, the name is unimportant
42 * Registry_Desc main_desc;
43 *
44 * Int main(Int argc, String argv[]) {
45 *
46 * //Register this file as a module "main"
47 * Registry_addModule(&main_desc, "main");
48 * @p 49 *
50 * Once registered, the legacy code may call log APIs without any other change
51 * and the formatted log events will show as coming from the registered
52 * modules. Also, the logging by the legacy code is now filtered by its own
53 * diags mask. The bits of this mask can be set using the Diags_setMask API.
54 *
55 * Continuing the previous example:
56 * @p(code) 57 * //Initialize the legacy code's diags mask to enable USER1.
58 * Diags_setMask("main=1");
59 * @p 60 *
61 * All events logged registered modules will be sent to the logger configured
62 * for the Registry module. For example, to configure the logger for use by
63 * all modules in the Registry:
64 * @p(code) 65 * Registry.common$.logger = LoggerBuf.create();
66 * @p 67 *
68 * There is no way to statically configure the diags masks for individual
69 * registered modules, since the registered modules are not known until
70 * runtime. However, it is possible to configure diags categories to be
71 * permanently off or on for ALL registered modules. This is done by
72 * configuring the diags mask for the xdc.runtime.Registry module. Diags
73 * categories set to ALWAYS_OFF will be permanently off for all Registry
74 * modules. Categories set to ALWAYS_ON will be permanently on for all
75 * Registry modules.
76 *
77 * In order to enable runtime configuration of individual Registry module
78 * masks, all relevant diags categories must be set to RUNTIME_OFF or
79 * RUNTIME_ON in the Registry module's mask.
80 */
81 @CustomHeader
82 module Registry
83 {
84 /*!
85 * ======== Result ========
86 * Status code returned from {@link addModule}.
87 *
88 * SUCCESS - The module was added successfully.
89 * ALLOC_FAILED - Unused.
90 * ALREADY_ADDED - The module has already been added or another module
91 * with the same name is present. The Registry will not
92 * be modified.
93 * ALL_IDS_USED - There are no more module ids available for new modules.
94 * There are a total of 16,384 - 1 module ids available for
95 * use by the Registry.
96 */
97 enum Result {
98 SUCCESS,
99 ALLOC_FAILED,
100 ALREADY_ADDED,
101 ALL_IDS_USED
102 };
103
104 /*! Registry module descriptor */
105 typedef Types.RegDesc Desc;
106
107 /*!
108 * ======== addModule ========
109 * Add a runtime module to the registry with the specified name.
110 *
111 * The 'desc' parameter and the 'modName' string provided must both be
112 * permanent since the Registry will maintain references to both of these.
113 *
114 * Returns a status code indicating success or the cause of failure. See
115 * {@link Result} for details.
116 */
117 Result addModule(Desc *desc, String modName);
118
119 /*!
120 * ======== findByName ========
121 * Find the registered module with the given name.
122 */
123 Desc *findByName(String name);
124
125 /*!
126 * ======== findByNamePattern ========
127 * @_nodoc 128 * Find all registered modules matching the specified pattern.
129 *
130 * This API is intended for use by Diags_setMask.
131 *
132 * The name pattern can be an exact module name or it can contain '%'
133 * as a wildcard. The 'len' parameter is the string length of the pattern.
134 *
135 * This function returns one module at a time, but can be called
136 * repeatedly to find all modules matching the pattern. On the first
137 * call, pass NULL as the 'prev' parameter. In all following calls,
138 * pass the last returned descriptor. This function returns NULL when
139 * it can't find any more modules matching the name pattern.
140 */
141 Desc *findByNamePattern(String namePat, Int len, Desc *prev);
142
143 /*!
144 * ======== findById ========
145 * Find registered module's descriptor from it's module ID.
146 */
147 Desc *findById(Types.ModuleId mid);
148
149 /*!
150 * ======== getMask ========
151 * Get the named registered module's diagnostic mask.
152 */
153 Bool getMask(String name, Types.DiagsMask *mask);
154
155 /*!
156 * ======== isMember ========
157 * Determines if the specified module ID belongs to a registered module.
158 *
159 * This function returns TRUE if and only if the specified module id
160 * is a valid Registry module id. It does not search the Registry for the
161 * module id, but simply checks if the id is within the range of valid
162 * Registry module ids.
163 */
164 Bool isMember(Types.ModuleId mid);
165
166 /*!
167 * ======== getNextModule ========
168 * API for walking the list of modules in the Registry.
169 *
170 * This API retrieves the next module in the Registry's module list. To
171 * get the head of the list, pass NULL. This API returns NULL when there
172 * are no more module's in the list.
173 */
174 Desc *getNextModule(Desc *desc);
175
176 /*!
177 * ======== getModuleName ========
178 * Get the module name associated with this module descriptor.
179 */
180 Char *getModuleName(Desc *desc);
181
182 /*!
183 * ======== getModuleId ========
184 * Get the module id associated with this module descriptor.
185 */
186 Types.ModuleId getModuleId(Desc *desc);
187
188 internal:
189
190 Desc *findByNameInList(String name, Desc *listHead);
191 Void newModule(Desc *desc, String modName);
192 Bool matchPattern(String pattern, Int len, String modName);
193
194 /*
195 * ======== Module_State ========
196 */
197 struct Module_State {
198 Desc *listHead;
199 Types.ModuleId curId;
200 }
201 }
202 /*
203 * @(#) xdc.runtime; 2, 1, 0,279; 5-27-2010 16:42:31; /db/ztree/library/trees/xdc/xdc-v38x/src/packages/
204 */
205