From RTSC-Pedia

Jump to: navigation, search
revision tip
—— LANDSCAPE orientation
[printable version]  [offline version]offline version generated on 02-Oct-2009 22:10 UTC

XDCscript - Template-Object.genFile

Generate textual output file from a template

Contents

Synopsis

 
 
var tplt = xdc.loadTemplate(templateFile);
tplt.genFile(outputFile, thisObj, args, clobber);

Parameters

outputFile 
string name of the output file to be created
thisObj 
object that is referenced within the template body via this
args 
array of arguments referenced within the template body via $args
clobber 
boolean which, if true, causes genFile to overwrite outputFile even if the contents of an existing file are identical to the template output

Description

Generates output to a specified file, which is created if necessary. Unless clobber is true, an existing file is overwritten only when its content has truly changed. Internally calls genStream().

See also

XDCscript - Template-Body Contents of the template file
XDCscript - Template-Object.genStream Generate textual output stream from a template

[printable version]  [offline version]offline version generated on 02-Oct-2009 22:10 UTC
Copyright © 2008 The Eclipse Foundation. All Rights Reserved


Views
Personal tools
package reference