From RTSC-Pedia

Jump to: navigation, search
revision tip
—— LANDSCAPE orientation
[printable version]  [offline version]offline version generated on 02-Oct-2009 22:10 UTC 

Demo of the RTSC Platform Wizard in CCSv4

Using CCStudio v4 to create a custom RTSC platform


RTSC Platform Wizard Demo Part 1: The following Flash demo shows how to use the RTSC platform wizard in CCSv4 to create a custom RTSC platform package.

When the demo pauses, click "Next" to continue. A table of contents at the end lets you review specific actions. If you don't see the demos, you can download the Flash player, or save the demo to disk.

 

RTSC Platform Wizard Demo Part 2: Next, you can continue to the second demo in this series shows how to further customize the memory sections defined for a platform package. It also shows how to reopen and rebuild a platform package you have created.

RTSC Platform Wizard Demo Part 3: The third demo in this series shows the files in a custom RTSC platform package and the zip file you can use to distribute the package.

See also

Demo of Customizing Memory Sections Editing a platform package and defining your own memory sections
Demo Showing Files in a Custom Plaform Package Platform package directory contains zip file for distribution
Demo Building with Custom Platform Package Set RTSC configuration project properties and compare a platform to a generated map file
RTSC+CCStudio v4 QuickStart Using CCStudio v4 to create, build, and debug RTSC projects
RTSC+Eclipse FAQs Using RTSC with Eclipse-Based Tools
XGCONF User's Guide Using the RTSC Graphical Configuration Tool in CCSv4

[printable version]  [offline version]offline version generated on 02-Oct-2009 22:10 UTC 
Copyright © 2008 The Eclipse Foundation. All Rights Reserved
Views
Personal tools
package reference