From RTSC-Pedia

Jump to: navigation, search
revision tip
—— LANDSCAPE orientation
[printable version]  [offline version]offline version generated on 02-Oct-2009 22:10 UTC

Command - xdc.tools.cdoc

Package documentation tool

Contents

Synopsis

 
xs xdc.tools.cdoc [options ...]

For a complete description of this tool's options, see its static Cdoc reference page xdc.tools.cdoc. Alternatively, you can always view this reference documentation using the interactive version of this tool (xdc.tools.cdoc.sg) from the command line.

    % xs xdc.tools.cdoc.sg xdc.tools.cdoc

Description

In addition to viewing reference documentation interactively as described in Using the CDOC reference help system, you can run a "batch" version of the CDOC tool to generate static HTML files for any collection of packages. After generating static pages, you can leverage popular search tools such as Google Desktop to locate relevant documentation or use a tool like htmldoc to create a single PDF reference manual.

Examples

Suppose for example that you have packages installed in the repositories c:/bios_6_00/packages and c:/codec_engine_1_20/packages. The following command generates configuration documentation for all of these packages and places it into the output directory named ref_html.

    xs xdc.tools.cdoc -od:ref_html -Pr c:/bios_6_00/packages c:/codec_engine_1_20/packages
[printable version]  [offline version]offline version generated on 02-Oct-2009 22:10 UTC
Copyright © 2008 The Eclipse Foundation. All Rights Reserved


Views
Personal tools
package reference