From RTSC-Pedia

Jump to: navigation, search
revision tip
—— LANDSCAPE orientation
[printable version]  [offline version]offline version generated on 02-Oct-2009 22:10 UTC

C - Module setMask

Set a module's diagnostics mask

Contents

Synopsis

 
 
 
#include <«pkg»/«Mod».h>
 
Void «Mod»_Module_setMask(Bits16 mask) /* set the value of «Mod»'s diagnostic mask */

Description

Every module «Mod» provides a parameterless macro named «Mod»_Module_setMask() that sets the current value of the module's diagnostics mask. If the module «Mod» does not have a mask, this method has no effect.

Since

This method was introduced in XDCtools release 3.15.

See also

C - Module_hasMask Check for a module diagnostics mask
C - Module_getMask Get a module's diagnostics mask

[printable version]  [offline version]offline version generated on 02-Oct-2009 22:10 UTC
Copyright © 2008 The Eclipse Foundation. All Rights Reserved


Views
Personal tools
package reference