1 /* --COPYRIGHT--,ESD
2 * Copyright (c) 2008 Texas Instruments. All rights reserved.
3 * This program and the accompanying materials are made available under the
4 * terms of the Eclipse Public License v1.0 and Eclipse Distribution License
5 * v. 1.0 which accompanies this distribution. The Eclipse Public License is
6 * available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
7 * Distribution License is available at
8 * http://www.eclipse.org/org/documents/edl-v10.php.
9 *
10 * Contributors:
11 * Texas Instruments - initial implementation
12 * --/COPYRIGHT--*/
13 /*
14 * ======== GateThread.xdc ========
15 */
16
17 import xdc.runtime.IGateProvider;
18 import xdc.runtime.knl.IGateThreadSupport;
19
20 /*!
21 * ======== GateThread ========
22 * Provides protection of critical sections across threads. [EXPERIMENTAL]
23 *
24 * This module provides services through its proxy
25 * IGateThreadSupport interface. It has a module wide config parameter
26 * {@link #Proxy} which needs to be bound to an OS specific delegate before
27 * this module can be used.
28 *
29 * Here is an example showing how the proxy is bound to an BIOS 6.x specific
30 * delegate.
31 *
32 * var GateThread = xdc.useModule('xdc.runtime.knl.GateThread');
33 * GateThread.Proxy =
34 * xdc.useModule('ti.sysbios.xdcruntime.GateThreadSupport');
35 *
36 * Typically the package containing the delegates have a Settings module that
37 * will bind all {@link xdc.runtime.knl} proxies. The following
38 * example sets up all the xdc.runtime.knl proxies.
39 *
40 * xdc.useModule("ti.sysbios.xdcruntime.Settings");
41 *
42 */
43
44 @InstanceInitError /* because initialization can fail */
45 @InstanceFinalize /* have to Gate_Proxy_delete(sem) on delete */
46
47 module GateThread inherits IGateProvider
48 {
49 /*! Proxy that needs to be bound to an OS specific delegate. */
50 proxy Proxy inherits IGateThreadSupport;
51
52 internal:
53
54 struct Instance_State {
55 Proxy.Handle proxyHandle;
56 }
57
58 }
59
60 /*
61 *! Revision History
62 *! ================
63 *! 17-Apr-2009 nitya Review updates
64 */
65 /*
66 * @(#) xdc.runtime.knl; 1, 0, 0,49; 6-21-2010 15:09:09; /db/ztree/library/trees/xdc/xdc-u19x/src/packages/
67 */
68