1 /* --COPYRIGHT--,ESD
2 * Copyright (c) 2008 Texas Instruments. All rights reserved.
3 * This program and the accompanying materials are made available under the
4 * terms of the Eclipse Public License v1.0 and Eclipse Distribution License
5 * v. 1.0 which accompanies this distribution. The Eclipse Public License is
6 * available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
7 * Distribution License is available at
8 * http://www.eclipse.org/org/documents/edl-v10.php.
9 *
10 * Contributors:
11 * Texas Instruments - initial implementation
12 * --/COPYRIGHT--*/
13 /*
14 * ======== Startup.xdc ========
15 *
16 *! Revision History
17 *! ================
18 *! 14-Dec-2007 sasha moved comments from the internal section to
19 * implemenation
20 */
21
22 package xdc.runtime;
23
24 /*!
25 * ======== Startup ========
26 * The `xdc.runtime` startup bootstrap
27 *
28 * Every module can optionally define a startup function which is called
29 * before `main()`. Modules declare that they want to participate in this
30 * startup sequence via the `@ModuleStartup` attribute in the module's spec
31 * file. Modules that use this attribute must also implement the following
32 * startup function:
33 * @p(code) 34 * Int Mod_Module_startup(Int state);
35 * @p 36 * where "Mod" is the name of the module requesting startup support.
37 *
38 * The parameter to the startup function serves as "state variable" whose
39 * initial value will be `Startup_NOTDONE`. If `startup()` returns a value
40 * other than `Startup_DONE`, it will be called in a subsequent pass with this
41 * return value passed in as `state`. To ensure this process terminates,
42 * no startup function is ever called more than `{@link #maxPasses}`
43 * times.
44 *
45 * For situations in which the startup of one module depends upon another
46 * having completed its startup processing, the following function is
47 * automatically defined for all modules and proxies:
48 * @p(code) 49 * Bool Mod_Module_startupDone();
50 * @p 51 * where "Mod" is the name of some module or proxy. These predicates can
52 * be used as guards inside of a startup function to probe whether a
53 * particular module has completed its own startup processing. As a
54 * convenience, the function `Startup_rtsDone()` probes the necessary set of
55 * `xdc.runtime` modules required to support instance `create()` functions, and
56 * should be called before any startup-time instance creation and/or
57 * memory allocation is performed.
58 * @p(code) 59 * Int Mod_Module_startup(Int state)
60 * {
61 * if (!Startup_rtsDone()) {
62 * return (Startup_NOTDONE);
63 * }
64 * .
65 * .
66 * .
67 * return (Startup_DONE);
68 * }
69 * @p 70 *
71 * @a(Startup Sequence) 72 * The following list defines when in the startup sequence the user provided
73 * startup functions are being invoked:
74 * @p(nlist) 75 * - CPU is initialized and C stack setup is performed.
76 * - Function specified by `Startup.resetFxn` is called.
77 * `Startup.resetFxn` is called only on platforms where reset is performed
78 * before running a program. For example, boot code for all TI targets
79 * invokes `Startup.resetFxn`, while that function is not invoked on
80 * Microsoft targets.
81 * - C runtime initialization is performed.
82 * - Functions from the array `Startup.firstFxns` are called.
83 * - All `Mod_Module_startup` functions are called in a loop until all such
84 * functions return `Startup_DONE` or `maxPasses` threshold is reached.
85 * - Functions from the array `Startup.lastFxns` are called.
86 * - The function `main` is called.
87 * @p 88 * The steps 4 - 6 occur during C++ static object initialization. Since
89 * the ANSI C++ Language Standard does not provide a means to control
90 * the order of C++ constructors, if a C++ constructor uses an XDC module,
91 * there is no guarantee that the module's startup function already ran.
92 * Therefore, any C++ constructor that needs XDC modules' services should
93 * call `Startup_exec` first to force all startup related functions from
94 * steps 4 - 6 to run, before the constructor uses any XDC module.
95 * @p 96 * Also, if a target does not support C++, the steps 4 - 6 will not run
97 * automatically. It is then up to a user's code to invoke `Startup_exec`,
98 * possibly as the first step in `main`.
99 * @p 100 */
101 @Template("./Startup.xdt")
102
103 module Startup {
104
105 /*!
106 * ======== DONE ========
107 * Returned from module startup functions no further calls are required
108 */
109 const Int DONE = -1;
110
111 /*!
112 * ======== NOTDONE ========
113 * Initial value of state argument passed to module startup functions
114 */
115 const Int NOTDONE = 0;
116
117 /*!
118 * ======== maxPasses ========
119 * Max number of iterations over the set of startup functions
120 */
121 config Int maxPasses = 32;
122
123 /*!
124 * ======== InitFxn ========
125 * Type of function assignable to `firstFxns`, `lastFxns`, or `resetFxn`
126 */
127 typedef Void (*InitFxn)();
128
129 /*!
130 * ======== firstFxns ========
131 * List of functions called before module startup
132 *
133 */
134 config InitFxn firstFxns[length] = [];
135
136 /*!
137 * ======== lastFxns ========
138 * List of functions called after module startup
139 *
140 */
141 config InitFxn lastFxns[length] = [];
142
143 /*!
144 * ======== resetFxn ========
145 * Function to be called by during initialization
146 *
147 * This function is called only on platforms where reset is performed
148 * before running the program. The purpose of this function is to set up
149 * the hardware registers (cache, external memory interface, etc.) before
150 * any other code executes.
151 *
152 */
153 metaonlyconfig InitFxn resetFxn = null;
154
155 /*!
156 * ======== exec ========
157 * Execute the startup functions of all resident modules
158 *
159 * Note that this function is idempotent, and can be called at any point
160 * in the platform/target startup sequence in which "ordinary" C functions
161 * can execute. By default, this function is called as part of the
162 * standard C++ static initialization sequence.
163 *
164 * If your target compiler does not support C++, this function must be
165 * called at least once prior to using any `xdc.runtime` modules.
166 * Simply call this function at the very beginning of `main()`.
167 */
168 Void exec();
169
170 /*!
171 * ======== rtsDone ========
172 * Query the state of the `xdc.runtime` package
173 *
174 * This function is used by module startup functions to determine
175 * when it is possible to use the `xdc.runtime` modules; e.g. to
176 * allocate memory, create instances managed by some module (even
177 * those outside the `xdc.runtime` package), call a `Log` function,
178 * etc.
179 *
180 * @a(returns) 181 * Returns `TRUE` when all `xdc.runtime` modules have completed
182 * initialization.
183 */
184 Bool rtsDone();
185
186 internal:
187
188 /*!
189 * ======== reset ========
190 * Application-specific reset function
191 *
192 * This function is defined in `Startup.xdt`
193 * (`xdc_runtime_Startup_reset__I`) and is called as early as
194 * possible in the program initialization process; for many platforms,
195 * it is called prior the the initialization of the C runtime
196 * environment.
197 */
198 Void reset();
199
200 Void startMods(Int state[], Int len);
201 readonlyconfig Void (*startModsFxn)(Int[], Int) = startMods;
202
203 extern Void execImplFxn() = xdc_runtime_Startup_exec__I;
204
205 readonlyconfig Void (*execImpl)() = execImplFxn;
206
207 typedef Int (*SFxn)(Int);
208 config SFxn sfxnTab[];
209
210 /*!
211 * ======== sfxnRts ========
212 * Array of runtime modules' startup functions
213 *
214 * This array also contains startup functions of the modules that inherit
215 * from interfaces in `xdc.runtime`. Functions added to this array are
216 * called only once before the startup procedure for all modules begins.
217 */
218 config Bool sfxnRts[];
219
220 struct Module_State {
221 Int *stateTab; /* initially null */
222 Bool execFlag; /* if true, startup code processing started */
223 Bool rtsDoneFlag;
224 };
225
226 }
227 /*
228 * @(#) xdc.runtime; 2, 0, 0, 0,240; 6-21-2010 15:09:09; /db/ztree/library/trees/xdc/xdc-u19x/src/packages/
229 */
230