1 /* --COPYRIGHT--,ESD
2 * Copyright (c) 2008 Texas Instruments. All rights reserved.
3 * This program and the accompanying materials are made available under the
4 * terms of the Eclipse Public License v1.0 and Eclipse Distribution License
5 * v. 1.0 which accompanies this distribution. The Eclipse Public License is
6 * available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
7 * Distribution License is available at
8 * http://www.eclipse.org/org/documents/edl-v10.php.
9 *
10 * Contributors:
11 * Texas Instruments - initial implementation
12 * --/COPYRIGHT--*/
13 /*!
14 * ======== IInstance ========
15 * Common instance params
16 *
17 * Every module's instance parameter structure contains a pointer to an
18 * `IInstance.Params` structure named `instance`. So, every instance
19 * parameter defined in this interface may optionally be set when
20 * creating (or constructing) any module's instances.
21 */
22 interface IInstance {
23
24 instance:
25
26 /*!
27 * ======== name ========
28 * Name of the instance
29 *
30 * It is possible to "bind" a name to each instance of any module
31 * at the time the instance is created (or constructed).
32 * @p(code) 33 * ModA_Params params;
34 * ModA_Params_init(¶ms);
35 * params.instance->name = "myInstance";
36 * ModA_create(¶ms, NULL);
37 * @p 38 *
39 * The name field must be assigned a pointer to a buffer that persists
40 * as long as the instance that it names exists. Only a reference to
41 * the name is retained in the instance, the name is not copied to a
42 * secondary buffer.
43 *
44 * If instances have been configured to not support names, it is still
45 * possible to assign to the `instance.name` field of the parameter
46 * structure (as shown above). However, the pointer is not retained
47 * and methods that normally return an instance's name will return
48 * `NULL` instead.
49 */
50 config String name = null;
51 }
52 /*
53 * @(#) xdc.runtime; 2, 0, 0, 0,239; 6-9-2010 16:24:58; /db/ztree/library/trees/xdc/xdc-u18x/src/packages/
54 */
55