1 /* --COPYRIGHT--,ESD
2 * Copyright (c) 2008 Texas Instruments. All rights reserved.
3 * This program and the accompanying materials are made available under the
4 * terms of the Eclipse Public License v1.0 and Eclipse Distribution License
5 * v. 1.0 which accompanies this distribution. The Eclipse Public License is
6 * available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
7 * Distribution License is available at
8 * http://www.eclipse.org/org/documents/edl-v10.php.
9 *
10 * Contributors:
11 * Texas Instruments - initial implementation
12 * --/COPYRIGHT--*/
13 /*
14 * ======== IHeap.xdc ========
15 *
16 *! Revision History
17 *! ================
18 *! 08-Jun-2007 nitya Fixed 14574: removed nodoc from create
19 *! 12-Dec-2006 tdm Added isBlocking api
20 *! 07-Nov-2005 tdm xdoc tweaks
21 *! 31-Oct-2005 tdm Started rev history and added Size
22 *! - if we ever change the name of this interface, we shoould change it to
23 *! IMemoryProvider
24 */
25
26 /*!
27 * ======== IHeap ========
28 * Interface to heap functions.
29 *
30 * All heap implementations inherit from this interface.
31 * The implementations can have additional configuration
32 * parmeters and functions.
33 *
34 */
35 interface IHeap {
36
37 instance:
38
39 /*!
40 * ======== alloc ========
41 * Allocates a block of memory from the heap.
42 *
43 * This method returns a block of memory from the heap.
44 * It is called by the `{@link xdc.runtime.Memory#alloc()}` function.
45 *
46 * @param(size) size (in MADUs) of the block
47 * @param(align) alignment (in MADUs) of the block
48 * @param(eb) pointer to error block
49 *
50 * @a(returns) Returns the address of the allocated memory.
51 */
52 Ptr alloc(SizeT size, SizeT align, Error.Block *eb);
53
54 /*!
55 * ======== create ========
56 * Create a heap.
57 *
58 * See specific `IHeap` implementation for parameters used.
59 */
60 create();
61
62 /*!
63 * ======== free ========
64 * Free a block of memory back to the heap.
65 *
66 * This method gives back a block of memory to a heap.
67 * It is called by the `{@link xdc.runtime.Memory#free()}` function.
68 *
69 * @param(block) non-`NULL` address of allocated block to free
70 * @param(size) size (in MADUs) of the block of memory to free
71 */
72 Void free(Ptr block, SizeT size);
73
74 /*!
75 * ======== isBlocking ========
76 * Returns whether the heap may block during an `{@link #alloc()}` or
77 * `{@link #free()}`.
78 *
79 * @a(returns) If the heap might block, `TRUE` is returned.
80 * If the heap does not block, `FALSE` is returned.
81 */
82 Bool isBlocking();
83
84 /*!
85 * ======== getStats ========
86 * Retrieve the statistics from the heap.
87 *
88 * The caller passes in a pointer to a `{@link xdc.runtime.Memory#Stats}`
89 * structure and `getStats` fills in this structure.
90 *
91 * This function is called by the `{@link xdc.runtime.Memory#getStats()}`
92 * function.
93 *
94 * @param(stats) non-`NULL` pointer to an output buffer
95 */
96 Void getStats(Memory.Stats *stats);
97 }
98 /*
99 * @(#) xdc.runtime; 2, 0, 0, 0,239; 6-9-2010 16:24:58; /db/ztree/library/trees/xdc/xdc-u18x/src/packages/
100 */
101