1 requires xdc.platform [1,0,1];
2
3 /*!
4 * ======== xdc.platform.generic ========
5 * Platform package for the generic platform.
6 *
7 * This package implements the interfaces (xdc.platform.IPlatform)
8 * necessary to build and run executables on a "generic" platform; a
9 * platform specified by:
10 * @p(blist) 11 * - device name; e.g., "TMS320C2812"
12 * - catalog name; the name of a package containing the device named above
13 * - clock rate; the clock rate in MHz of the CPU
14 * - external memory map; an array of memory blocks external to the device
15 * @p 16 * For a complate list of parameters that can be specified when creating a
17 * platform instance see the instance configuration parameters specified
18 * by `{@link xdc.platform.generic.Platform}`. This list, of course,
19 * includes all the instance config parameters specified by the
20 * `{@link xdc.platform.IPlatform}` interface.
21 *
22 * @a(Throws) 23 * `XDCException` exceptions are thrown for fatal errors. The following error
24 * codes are reported in the exception message:
25 * @p(dlist) 26 * - `xdc.platform.generic.LINK_TEMPLATE_ERROR`
27 * This error is raised when this platform cannot found the default
28 * linker command template `linkcmd.xdt` in the build target's
29 * package. When a target does not contain this file, the config
30 * parameter `{@link xdc.cfg.Program#linkTemplate}` must be set.
31 * @p 32 *
33 * @a(EXAMPLES) 34 * Example 1: Suppose you need to create an application for a HW platform
35 * that uses the TMS320C2812 running at 150 MHz. You can use this package
36 * (in lieu of one specifically created for the HW platform) by defining a
37 * named instance of this package's Platform module. Add the following
38 * statements to your `config.bld` file to add the platform instance named
39 * "xdc.platform.generic:C28".
40 * @p(code) 41 * Build.platformTable["xdc.platform.generic:C28"] = {
42 * clockRate: 150,
43 * catalogName: "ti.catalog.c2800",
44 * deviceName: "TMS320C2812"
45 * };
46 * @p 47 * With this name defined, it is now possible to configure an application
48 * using the platform instance name "xdc.platform.generic:C28". For example,
49 * if you are using `{@link xdc.tools.configuro}` to configure your
50 * application, the string "xdc.platform.generic:C28" can now be used to
51 * identify your platform:
52 * @p(code) 53 * xs xdc.tools.configuro -b config.bld -p xdc.platform.generic:C28 ...
54 * @p 55 *
56 * @p(html) 57 * <hr/>
58 * @p 59 *
60 * Example 2: The following example illustrates how to specify a platform
61 * instance with memory regions external to the specified device. In this
62 * case, we define a platform using a TMS320C6416 running at 600 MHz on a
63 * board with two external SDRAM memory blocks.
64 * @p(code) 65 * Build.platformTable["xdc.platform.generic:C64"] = {
66 * clockRate: 600,
67 * catalogName: "ti.catalog.c6000",
68 * deviceName: "TMS320C6416",
69 * externalMemoryMap : [
70 * ["SDRAM1", {
71 * name: "SDRAM1",
72 * base: 0x80000000, len: 0x1000000, space: "code/data"
73 * }],
74 * ["SDRAM2", {
75 * name: "SDRAM2",
76 * base: 0x90000000, len: 0x1000000, space: "code/data"
77 * }],
78 * ]
79 * }
80 * @p 81 *
82 * The `externalMemoryMap` attribute is a map of string names to
83 * `{@link xdc.platform.IPlatform#Memory}` structures.
84 *
85 * @see xdc.platform.generic.Platform
86 * @see xdc.bld.BuildEnvironment#platformTable
87 * @see xdc.platform.IPlatform
88 */
89 package xdc.platform.generic [1,0,0] {
90 module Platform;
91 }
92 /*
93 * @(#) xdc.platform.generic; 1, 0, 0,48; 6-9-2010 16:24:43; /db/ztree/library/trees/xdc/xdc-u18x/src/packages/
94 */
95