1 /* --COPYRIGHT--,EPL
2 * Copyright (c) 2008 Texas Instruments and others.
3 * All rights reserved. This program and the accompanying materials
4 * are made available under the terms of the Eclipse Public License v1.0
5 * which accompanies this distribution, and is available at
6 * http://www.eclipse.org/legal/epl-v10.html
7 *
8 * Contributors:
9 * Texas Instruments - initial implementation
10 *
11 * --/COPYRIGHT--*/
12 /*
13 * ======== Utils.xdc ========
14 */
15
16 package xdc.platform;
17
18 /*!
19 * ======== Utils ========
20 * Misc platform utilities
21 */
22 metaonlymodule Utils
23 {
24 /*!
25 * ======== assembleMemoryMap ========
26 * Combine the device and the external memory map into a platform map
27 *
28 * This function combines memory maps and also applies memory map name
29 * changes requested through renameMap.
30 *
31 * @param(cpu) an `xdc.platform.IExeContext` object
32 *
33 * @param(plat) a platform instance
34 *
35 * @param(noCheck) if true, and a custom memory map is defined, the
36 * function does not check if the custom memory map fits
37 * into the available physical memory
38 *
39 * @a(returns) platform memory map
40 */
41 function assembleMemoryMap(cpu, plat, noCheck);
42
43 /*!
44 * ======== checkDefaults ========
45 * Check if dataMemory, codeMemory and stackMemory are set correctly
46 *
47 * The `xdc.platform.IPlatform` instance parameters 'dataMemory',
48 * 'codeMemory', and 'stackMemory' are strings. This function verifies
49 * that those strings correspond to names of the memory objects in the
50 * supplied memory map.
51 *
52 * @param(inst) an `xdc.platform.IPlatform` instance
53 *
54 * @param(memMap) a map of `xdc.platform.IPlatform.Memory` objects
55 *
56 * @a(returns) 'true' if checked parameters are valid, 'false'
57 * otherwise
58 */
59 function checkDefaults(inst, memMap);
60
61 /*!
62 * ======== checkFit ========
63 * Check if a memory map fits into available physical memory
64 *
65 * A custom memory map segment can be spread over multiple physical
66 * memories or multiple custom memory map segments can be located in
67 * one physical memory. However, code/data restrictions must be followed.
68 * A custom memory segment with the parameter 'space' set to "code/data",
69 * which is the default value if the parameter was not specified, can fit
70 * only into "code/data" physical memories. Custom memory segments with
71 * 'space' set to "code" can fit into "code" and "code/data" memories, and
72 * custom memory segments with 'space' set to "data" can fit into "data"
73 * and "code/data" physical memories.
74 *
75 * @param(realMemMap) a map of `xdc.platform.IPlatform.Memory`
76 * objects containing physical memory map as
77 * defined in datasheets for the device and the
78 * platform
79 *
80 * @param(customMemMap) a map of `xdc.platform.IPlatform.Memory`
81 * objects containing user defined memory map,
82 * which must fit within boundaries of 'realMemMap'
83 *
84 * @a(returns) 'true', if customMemMap fits within realMemMap,
85 * and 'false' otherwise
86 */
87 function checkFit(realMemMap, customMemMap);
88
89 /*!
90 * ======== checkOverlap ========
91 * Check if there is an overlap among memory objects in a memory map
92 *
93 * @param(memMap) a map of `xdc.platform.IPlatform.Memory` objects
94 *
95 * @a(returns) a string with names of Memory objects that overlap
96 */
97 function checkOverlap(memMap);
98
99 /*!
100 * ======== getCpuDataSheet ========
101 * Get the specified cpu data sheet object
102 *
103 * @param(cpuDesc) an `xdc.platform.IExeContext.Cpu` object identifying
104 * the CPU device
105 *
106 * @a(returns) an `xdc.platform.ICpuDataSheet.Instance` object that
107 * corresponds to the specified cpuDesc
108 *
109 * @a(throws) `Error` exceptions are thrown for fatal errors
110 */
111 function getCpuDataSheet(cpuDesc);
112 }
113
114 /*
115 * @(#) xdc.platform; 1, 0, 1, 0,239; 6-9-2010 16:24:42; /db/ztree/library/trees/xdc/xdc-u18x/src/packages/
116 */
117