package xdc |
![](../Arrow_right.png) |
Core interfaces and modules necessary for the XDC runtime
In addition to the interfaces specified below, this package also supplies
a C/C++ header,
std.h that facilitates the creation of portable sources.
This header defines a set of "base" types that enable the creation
of C-code that is portable between any two targets. C source code that
relies exclusively on these types is portable to all targets and
platforms. Where appropriate, the types defined below are related to the
types defined in the library headers perscribed by the C99 standard
(ISO/IEC 9899:1999).
[
more ... ]
package xdc [1, 1, 1] {
// Base interface implemented by all packages
}
DETAILS
In addition to the interfaces specified below, this package also supplies
a C/C++ header, std.h that facilitates the creation of portable sources.
This header defines a set of "base" types that enable the creation
of C-code that is portable between any two targets. C source code that
relies exclusively on these types is portable to all targets and
platforms. Where appropriate, the types defined below are related to the
types defined in the library headers perscribed by the C99 standard
(ISO/IEC 9899:1999).
Why not simply use the C99 types? Having a
unique set of names provides a layer of insulation between a portable code
base and a particular compiler; e.g., even if a compiler does not support
the C99 types or defines them inappropriately for a particular device, it
is possible to use the compiler without changing the code base. Thus, the
developer is not forced to choose the lesser of two evils: waiting for a
change to the compiler or forking the code base for a particular compiler
device combination.
There are several situations where a small separate set of portable types
can help the maintainability of a code base.
- not all of the types described in the C99 standard are required to
be defined by conformant implementations nor is it possible for all
devices to implement some of the types specified (e.g., int8_t is
not implemented on C54 devices); so it is difficult to identify
non-portable source code.
- not all compilers provide C99 type support; if XDC supplies the type
definition and the compiler is updated to include C99 types, a
compilation error will occur if the source includes the C99
headers.
- not all compiler and device combinations are conformant; even high
quality compilers may not properly define the types for each device
supported by compiler.
USAGE
To compile sources that include xdc/std.h, two symbols must be defined
before including this header:
- xdc_target_types__
-
the package qualified path of the target's standard types header;
e.g., ti/targets/std.h. This value is specified in the target's
stdInclude config parameter; see
xdc.bld.ITarget.stdInclude
- xdc_target_name__
-
the target's module name without the package prefix; e.g., C64
rather than ti.targets.C64.
For example, to compile sources for the ti.targets.C64 target using TI's
cl6x compiler, the following command line is sufficient:
cl6x -Dxdc_target_types__=ti/targets/std.h -Dxdc_target_name__=C64
Each of the type names below has an equivalent "long name"; i.e., a name
that has an "xdc_" prefix. For example, the type Bool can also be
written as "xdc_Bool". Long names exist to avoid conflicts with
names defined or used by existing code bases.
In the event that one of the short type names below conflicts with another
type name (that can not be changed), it is possble to disable the short
names by defining the symbol xdc__nolocalnames before including
xdc/std.h.
#define xdc__nolocalnames
#include <xdc/std.h>
STANDARD TYPES
This header may be included multiple times and defines the following
target-dependent types:
- Bool
-
this type is large enough to hold the values 0 or 1. The
constants TRUE and FALSE are of this type; see below.
- String
-
this type is defined to be a char * and exists to allow code
to distinguish between pointers to buffers of raw data and
'\0' terminated strings.
- Intn, where n = 8, 16, or 32
-
signed integer type that is large enough to hold n bits; the
actual target type may by be larger than n. This type is
equivalent to one of the C99 types int_leastn_t or
int_fastn_t; see Section 7.18.
- UIntn, where n = 8, 16, or 32
-
unsigned integer type that is large enough to hold n bits; the
actual target type may by be larger than n. This type is
equivalent to one of the C99 types uint_leastn_t or
uint_fastn_t; see ISO/IEC 9899:1999 Section 7.18.
- Bitsn, where n = 8, 16, or 32
-
unsigned integer type that is precisely n bits. Not all targets
support all values of n; if the target does not support an exact
size the corresponding type is not defined. This type is
equivalent to the corresponding C99 type uintn_t; see ISO/IEC
9899:1999 Section 7.18.
- Fxn
-
this type is a pointer to code; it can hold a pointer to any
function.
- Ptr
-
this type is a pointer to data; it can hold a pointer to any
data structure.
- IArg
-
this integer type is large enough to hold a Fxn, Ptr, or
Int.
- UArg
-
this unsigned integer type is large enough to hold a Fxn,
Ptr, or Int.
- LLong
-
this long integer type is large enough to hold a Long and is
defined as a 'long long' type on targets that support this type;
otherwise, it is simply a Long.
Note that C99 requires the long long type to be at least 64-bits
wide (See ISO/IEC 9899:1999 Section 5.2.4.2.1). But some
compilers do not support 64-bit integral types and some don't
support the long long even though they do support 64-bit
integral types. Since these variations limit the portability of
valid C sources, the LLong type is always defined, is always at
least as wide as the Long type, and is at least 64-bits wide for
targets that support 64-bit integral types.
- ULLong
-
this unsigned long integer type is large enough to hold a ULong
and is defined as a 'unsigned long long' type on targets that
support this type; otherwise, it is simply a ULong.
The xdc/std.h header also defines the following aliases for the base C
types. These aliases exist so that C sources can consistently follow
a naming convention in which all type names are written in camel-case.
- Char and UChar
-
aliases for char and unsigned char, respectively
- Short and UShort
-
aliases for short and unsigned short, respectively
- Int and UInt
-
aliases for int and unsigned int, respectively
- Long and ULong
-
aliases for long and unsigned long, respectively
- Double and LDouble
-
aliases for double and long double, respectively
- SizeT
-
alias for size_t
- VaList
-
alias for va_list
The types above are defined for all targets. Some targets can support
the following additional types. Since these types are not always
supported by a target, these types should only be used when no other
type sufficies.
- Bitsn, where n = 8, 16, or 32
-
this unsigned integer type is precisely n-bits wide. This type is
equivalent to the optional C99 type uintn_t; see ISO/IEC
9899:1999 Section 7.18.1.1. This type is defined if and
only if the preprocessor macro xdc__BITSn__ is defined.
(64-Bit Types)
Although the C99 standard requires support for 64-bit types, not all
compiler/device combinations can usefully support them. As a result,
the 64-bit types described here may not be defined for all targets. For
each type there is a corresponding pre-processor macro which is
defined if and only if the type is supported.
- Int64
-
signed integer type that is large enough to hold 64 bits; the
actual target type may by be wider than 64 bits. This type is
equivalent to one of the C99 types int_least64_t or
int_fast64_t; see Section 7.18. This type is defined if and
only if the preprocessor macro xdc__INT64__ is defined.
- UInt64
-
unsigned integer type that is large enough to hold n bits; the
actual target type may by be wider than 64 bits. This type is
equivalent to one of the C99 types uint_least64_t or
uint_fast64_t; see ISO/IEC 9899:1999 Section 7.18. This type
is defined if and only if the preprocessor macro
xdc__INT64__ is defined.
- Bits64
-
unsigned integer type that is precisely 64 bits wide. If the target
does not support an exact 64-bit size, this type is not defined.
This type is equivalent to the corresponding C99 type
uint64_t; see ISO/IEC 9899:1999 Section 7.18. This type is
defined if and only if the preprocessor macro xdc__BITS64__ is
defined.
PREDEFINED MACROS
In addition to the type definitions above, xdc/std.h also defines the
following commonly used constants
- NULL
-
defined as 0
- TRUE
-
defined as ((Bool)1)
- FALSE
-
defined as ((Bool)0)
Finally, xdc/std.h defines the following target-independent symbols
that have target-dependent values; these predefined macros enable
conditional compilation of source files based on target-specific
attributes.
- {c_target_name}
-
this symbol (the target's fully qualified name with all '.'s
replaced with '_') is always defined and allows one to easily
include target-specific headers or define symbols with
target-specific values.
- xdc_target__isaCompatible_{isa_name}
-
for every ISA named in the array returned by this target's
xdc.bld.ITarget.getISAChain() method, a symbol of this
name is defined. In addition to enabling one to create code
specific to a particular ISA, this allows one to create code that
depends on TI's C6x architecture without being dependent
on a particular member of the C6x family, for example.
- xdc_target__isa_{isa}
-
this symbol is always defined and {isa} is the
target's isa (see xdc.bld.ITarget.isa).
- xdc_target__{little,big}Endian
-
if this target's xdc.bld.ITarget.model.endian property is
specified, this symbol is defined and {little,big} is replaced
by model.endian.
- xdc_target__{code_model_name}Code
-
if this target's xdc.bld.ITarget.model.codeModel is
specified, this symbol is defined and {code_model_name} is
replaced by model.codeModel.
- xdc_target__{data_model_name}Data
-
if this target's xdc.bld.ITarget.model.dataModel is
specified, this symbol is defined and {data_model_name} is
replaced by model.dataModel.
- xdc_target__os_{os_name}
-
this symbol is always defined and {os_name} is the
target's os name (see xdc.bld.ITarget.os).
- xdc_target__sizeof_{type_name}
-
this symbol is defined for each type name supported in the target's
xdc.bld.ITarget.stdTypes structure, {type_name} is the
name of one of the standard types supported above, and the
value is sizeof(type_name).
- xdc_target__alignof_{type_name}
-
this symbol is defined for each type name supported in the target's
xdc.bld.ITarget.stdTypes structure, {type_name} is the
name of one of the standard types supported above, and the
value is the alignment required by the compiler for {type_name}.
- xdc_target__bitPerChar
-
this symbol is always defined and specifies the number of bits
in the target's char. This value combined with the
xdc_target__sizeof_ values allows C code to determine the
precise number of bits in any of the standard types.
SEE
THROWS
XDCException exceptions are thrown for fatal errors. The following
error codes are reported in the exception message:
- xdc.PACKAGE_NOT_FOUND
-
This error is reported whenever a specified package is not found
This may happen for the following reasons:
- Ensure that the package in question is contained in one of
the repositories named in the package path.
- The package has not been built by the xdc tool even though
the physical package directory may be present along the
package path
- xdc.FILE_NOT_FOUND
-
This error is reported when a specified file is not found.
Ensure that any directory name prefix in the name is a package
directory contained in one of the repositories named in the
package path. For example, if "ti/targets/linkcmd.xdt" can't
be found, make sure the directory ti/targets/ is contained in
at least one repository named in the package path.
- xdc.MODULE_NOT_FOUND
-
This error is reported when a specified module can't be
found. Ensure that the package containing the module in
question is contained in at least one repository named in
the package path.
Also ensure that the module name is qualified with the
package name. For example, to refer to the module Engine
in the package ti.sdo.ce, the module name should be
specified as ti.sdo.ce.Engine.
- xdc.TOOL_USAGE_ERROR
-
This error may happen when the xs tool is not passed the
expected command line arguments.
- xdc.MODULE_UNDEFINED_MAIN_FUNCTION
-
This error is reported when the xs tool is passed a module
that does not define a main function. Ensure that the
meta-domain implementation of the module has a main function.
- xdc.SPEC_FILE_ERROR
-
This error is reported when there is a parsing error in a
specification file. Check the spec. file for syntax errors.
- xdc.DEPRECATED_FUNCTION
-
This error is reported whenever a deprecated function is called.
- xdc.STATIC_INSTANCE
-
This error is reported when a function create() is called at the
configuration time for a module that does not implement the
function instance$static$init and therefore does not support
static instances.
generated on Sat, 12 Jun 2010 05:52:01 GMT