1 /* --COPYRIGHT--,EPL
2 * Copyright (c) 2008 Texas Instruments and others.
3 * All rights reserved. This program and the accompanying materials
4 * are made available under the terms of the Eclipse Public License v1.0
5 * which accompanies this distribution, and is available at
6 * http://www.eclipse.org/legal/epl-v10.html
7 *
8 * Contributors:
9 * Texas Instruments - initial implementation
10 *
11 * --/COPYRIGHT--*/
12 /*
13 * ======== ICpuDataSheet.xdc ========
14 */
15 package xdc.platform;
16
17 /*!
18 * ======== ICpuDataSheet ========
19 * CPU information provided by the HW model.
20 *
21 * The information in this interface is read-only, defined by the chip's
22 * data sheet, and is obtained by naming a module in a package that
23 * implements this interface.
24 *
25 * Data sheets are created by platforms as part of creating an "execution
26 * context" (see `{@link xdc.platform.IPlatform#getExeContext}`). This
27 * execution context includes the CPU's memory map as well as any external
28 * memory provided by the platform itself, for example.
29 */
30 metaonlyinterface ICpuDataSheet
31 {
32
33 instance:
34 /*!
35 * ======== create ========
36 * Create a "data-sheet" for the specified revision of a CPU.
37 *
38 * A "data sheet" for a CPU allows one to get specific attributes
39 * for a CPU programatically; e.g., the memory map of the CPU.
40 *
41 * Notice that we don't specify CPU registers when we create a
42 * a data-sheet; registers are provided as necessary to the other
43 * functions defined in this interface. This allows one to more easily
44 * get memory maps for several different setting of the registers,
45 * for example.
46 *
47 * @param(revision) a string that identifies revision of the CPU to be
48 * created.
49 */
50 create(string revision);
51
52 /*!
53 * ======== cpuCore ========
54 * A string identifying the CPU Core.
55 *
56 * This uniquely identifies the instruction set that the CPU can
57 * decode and execute.
58 */
59 config string cpuCore; /* 5400, 5500, etc... */
60
61 /*!
62 * ======== cpuCoreRevision ========
63 * A string that uniquely identifies a revision of the core.
64 */
65 config string cpuCoreRevision; /* 1.2, 2.0, etc... */
66
67 /*!
68 * ======== minProgUnitSize ========
69 * The minimum addressable program unit size in 8-bit bytes
70 */
71 configint minProgUnitSize;
72
73 /*!
74 * ======== minDataUnitSize ========
75 * The minimum addressable data unit size in 8-bit bytes
76 */
77 configint minDataUnitSize;
78
79 /*!
80 * ======== dataWordSize ========
81 * The size of an int on the target in 8-bit bytes
82 */
83 configint dataWordSize;
84
85 /*!
86 * ======== getMemoryMap ========
87 * Get the memory map that corresponds to the values of the specified
88 * registers.
89 *
90 * If a register is not specified and this register can affect the
91 * memory map, the register is assumed to be set to its reset
92 * value (the value of the register immediately after a CPU reset).
93 *
94 * @param(registers) a hash of named registers to values at the time
95 * an executable is to be loaded (for example)
96 *
97 * @a(returns) Returns an array of
98 * `{@link xdc.platform.IPlatform#Memory}`
99 * objects that represent the memory visible to an
100 * executable running on the CPU.
101 */
102 // xdc.platform.IPlatform.Memory [] getMemoryMap(int registers [string]);
103 function getMemoryMap(registers);
104
105 /*!
106 * ======== getRegisterSet ========
107 * The set of valid register names for this CPU
108 *
109 * This function returns the complete set of register names that may be
110 * passed to the `{@link #getMemoryMap()}` function. This function is
111 * only used to enable one to write a "requires contract" for the
112 * `{@link #getMemoryMap()}` function.
113 *
114 * @a(returns) Returns an array of valid register names (strings) for
115 * this device; only names from this array are valid keys
116 * for the registers argument to `{@link #getMemoryMap()}`.
117 */
118 // string [] getRegisterSet();
119 function getRegisterSet();
120 };
121 /*
122 * @(#) xdc.platform; 1, 0, 1, 0,237; 2-22-2010 10:33:24; /db/ztree/library/trees/xdc/xdc-u17x/src/packages/
123 */
124