From RTSC-Pedia
revision tip
LANDSCAPE orientation[printable version] [offline version] | offline version generated on 02-Oct-2009 22:10 UTC |
XDCspec - @XmlDtd
This structure can be serialized as XML
This attribute is applicable to structures only. The meta-domain representation of structures with his attribute have a function named $xml() attached to them. This function returns an E4X XML representation of the object which can be used to easily serialize this structure within XML files.
[printable version] [offline version] | offline version generated on 02-Oct-2009 22:10 UTC |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved