From RTSC-Pedia
revision tip
LANDSCAPE orientation[printable version] [offline version] | offline version generated on 02-Oct-2009 22:10 UTC |
XDCspec - @GlobalNames
This module defines "unprefixed" identifiers
By default, the "short" prefix used to reference a module's methods is the module's name (without the package prefix) followed by a single underscore ('_'). For example, the short name of the ti.sysbios.knl.Task module's create method is Task_setPri. The GlobalNames attribute causes an additional set of short names to be defined in which even the module prefix is absent; if the ti.sysbios.knl.Task module had the GlobalNames attribute, rather then reference Task_setPri, clients could also simply reference setPri.
[printable version] [offline version] | offline version generated on 02-Oct-2009 22:10 UTC |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved