From RTSC-Pedia
revision tip
LANDSCAPE orientationXDCscript - xdc.loadTemplate
Create a template from a template file
Synopsis
| var templateObject = xdc.loadTemplate(templatePathName); |
Parameters
- templatePathName
- string file name of the template to be loaded; e.g., "my/template/pkg/foo.xdt" The template file is located via xdc.findFile().
Description
xdc.loadTemplate() loads a template file and returns a template object that can then be used to generate output either to a file or an output stream. This object has two methods that "expand" the template into either an existing output stream or into a new file.
- tplt.genFile(fileName, thisObj, args, clobber)
Generates output to fileName, which is created if necessary. Unless clobber is true, an existing file is overwritten only when its content has truly changed.
- tplt.genStream(outStream, thisObj, args)
Generates output to outStream, an instance of class java.io.PrintStream. All three parameters are passed to the underlying template generation function.
Return Value
xdc.loadTemplate returns a template object or throws an exception if the package can not be found or a syntax error occurs within the template file itself.
Example
Suppose the file header.xdt is a template for a C header that has an include guard based on the first argument of the argument array passed to the genFile method. The following code fragment will generate a file named "foo.h with an include guard based on the string "foo".
| foo.xs |
| var template = xdc.loadTemplate("header.xdt");
template.genFile("foo.h", this, ["foo"]); |
| | header.xdt |
| %%{
var NAME = $args[0];
%%}
/*
* ======== `NAME`.h =========
*/
#ifndef `NAME`_include
#define `NAME`_include 1
#endif /* `NAME`_include */ |
|
See also
Copyright © 2008 The Eclipse Foundation. All Rights Reserved