From RTSC-Pedia
revision tip
LANDSCAPE orientation[printable version] [offline version] | offline version generated on 02-Oct-2009 22:10 UTC |
XDCscript - Vector-Object.length
Get or set the number of values in a vector
Contents |
Synopsis
| var len = «vec».length; /* get the length of «vec» */ «vec».length = ...; /* set the length of «vec» */ |
Description
The length property of the vector «vec» can be used to get or set the number of typed values in «vec».
See also
XDCscript - Typed-Object | Objects specified by the RTSC Interface Definition Language |
XDCscript - Vector-Object | A typed JavaScript array |
[printable version] [offline version] | offline version generated on 02-Oct-2009 22:10 UTC |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved