From RTSC-Pedia
revision tip
LANDSCAPE orientation[printable version] [offline version] | offline version generated on 02-Oct-2009 22:10 UTC |
XDCscript - Typed-Object.$sealed
Test a typed object or one of its fields for being read-only
Contents |
Synopsis
| «tobj».$sealed(«fieldName») |
Description
Returns true if the specified field within «tobj» is sealed (read-only). If «fieldName» is omitted, returns true if the entire object is sealed.
See also
XDCscript - Typed-Object | Objects specified by the RTSC Interface Definition Language |
XDCscript - Typed-Object.$unseal | Unseal a typed object or one of its fields |
XDCscript - Typed-Object.$seal | Seal a typed object or one of its fields |
[printable version] [offline version] | offline version generated on 02-Oct-2009 22:10 UTC |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved