From RTSC-Pedia
revision tip
LANDSCAPE orientation[printable version] [offline version] | offline version generated on 02-Oct-2009 22:10 UTC |
XDCscript - Proxy-Object
Module object for a proxy
Contents |
Description
A proxy object is a module object for a module that is implicitly created during configuration and which simply delegates all method calls to a delegate module specified by a configuration script. Although the delegate and the proxy must inherit from the same interface, in general, the delegate module object and the proxy object have different types.
See Also
XDCscript - Module-Object | Object containing per-module-features of a module |
XDCscript - Proxy-Object.delegate$ | Module that implements the proxy's interface |
[printable version] [offline version] | offline version generated on 02-Oct-2009 22:10 UTC |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved