From RTSC-Pedia
revision tip
LANDSCAPE orientation[printable version] [offline version] | offline version generated on 02-Oct-2009 22:10 UTC |
XDCscript - Module-Object.$super
The interface from which this module inherits
Contents |
Synopsis
| «Mod».$super |
where «Mod» is a module object.
Description
The $super property of a meta-only module object is the interface object from which this module inherits. Since meta-only interfaces have default implementations of methods that are inherited by all inheriting modules, $super enables these modules to invoke the methods in the interface as part of their implementation.
[printable version] [offline version] | offline version generated on 02-Oct-2009 22:10 UTC |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved