From RTSC-Pedia
revision tip
LANDSCAPE orientation[printable version] [offline version] | offline version generated on 02-Oct-2009 22:10 UTC |
XDCscript - Instance-Object.$name
Canonical name for the instance
Contents |
Synopsis
| «inst».$name |
where «inst» is an instance object.
Description
The $name property of an instance object is the canonical name assigned to the instance by XDCscript when it is created.
See also
XDCscript - Instance-Object | Object containing per-instance-features of a module |
[printable version] [offline version] | offline version generated on 02-Oct-2009 22:10 UTC |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved