From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 02-Oct-2009 22:10 UTC | ![]() |
Demo Building with Custom Platform Package
Set RTSC configuration project properties and compare a platform to a generated map file
The Flash demo below shows how to specify the platform package that a RTSC configuration project should build with. It then builds the main project, which causes the referenced RTSC configuration project to also be built. In addition, this demo compares the memory sections defined in a custom platform package with the resulting memory sections in the .map file generated as part of the project build.
When the demo pauses, click "Next" to continue. A table of contents at the end lets you review specific actions.
If you don't see the demo, you can download the Flash player, or save the demo to disk.
See also
Demo of the RTSC Platform Wizard in CCSv4 | Using CCStudio v4 to create a custom RTSC platform |
Demo of Customizing Memory Sections | Editing a platform package and defining your own memory sections |
Demo Showing Files in a Custom Plaform Package | Platform package directory contains zip file for distribution |
Using Targets and Platforms | Introduction to targets and platforms |
![]() | [printable version] [offline version] | offline version generated on 02-Oct-2009 22:10 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved