From RTSC-Pedia
revision tip
LANDSCAPE orientation[printable version] [offline version] | offline version generated on 02-Oct-2009 22:10 UTC |
C - Module getMask
Get a module's diagnostics mask
Contents |
Synopsis
| #include <«pkg»/«Mod».h> Bits16 «Mod»_Module_getMask(void) /* get the value of «Mod»'s diagnostic mask */ |
Description
Every module «Mod» provides a parameterless macro named «Mod»_Module_getMask() that returns the current value of the module's diagnostics mask.
Since
This method was introduced in XDCtools release 3.15.
See also
C - Module_hasMask | Check for a module diagnostics mask |
C - Module_setMask | Set a module's diagnostics mask |
[printable version] [offline version] | offline version generated on 02-Oct-2009 22:10 UTC |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved