1 /* --COPYRIGHT--,ESD
2 * Copyright (c) 2008 Texas Instruments. All rights reserved.
3 * This program and the accompanying materials are made available under the
4 * terms of the Eclipse Public License v1.0 and Eclipse Distribution License
5 * v. 1.0 which accompanies this distribution. The Eclipse Public License is
6 * available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
7 * Distribution License is available at
8 * http://www.eclipse.org/org/documents/edl-v10.php.
9 *
10 * Contributors:
11 * Texas Instruments - initial implementation
12 * --/COPYRIGHT--*/
13 /*
14 * ======== Thread.xdc ========
15 */
16
17 import xdc.runtime.Error;
18 import xdc.runtime.Assert;
19 import xdc.runtime.knl.IThreadSupport;
20
21 /*!
22 * ======== Thread ========
23 * Thread services. [EXPERIMENTAL]
24 *
25 * This module manages threads through a proxy which inherits from
26 * IThreadSupport interface. It has a module wide config parameter
27 * {@link #Proxy} which needs to be bound to an OS specific delegate before
28 * this module can be used.
29 *
30 * Here is an example showing how the proxy is bound to a BIOS 6.x specific
31 * delegate.
32 *
33 * var Thread = xdc.useModule('xdc.runtime.knl.Thread');
34 * Thread.Proxy = xdc.useModule('ti.sysbios.xdcruntime.ThreadSupport');
35 *
36 * Typically a package containing the delegates has a Settings module that
37 * will bind all {@link xdc.runtime.knl} proxies. The following
38 * example sets up all the xdc.runtime.knl proxies.
39 *
40 * xdc.useModule('ti.sysbios.xdcruntime.Settings');
41 *
42 */
43
44 @InstanceInitError /* because initialization can fail */
45 @InstanceFinalize /* have to Thread_Proxy_delete(sem) on delete */
46
47 module Thread
48 {
49 /*! Thread priorities which are mapped to OS specific value by Proxy */
50 enum Priority {
51 Priority_INVALID,
52 Priority_LOWEST,
53 Priority_BELOW_NORMAL,
54 Priority_NORMAL,
55 Priority_ABOVE_NORMAL,
56 Priority_HIGHEST
57 };
58
59 /*! Invalid OS priority value */
60 const Int INVALID_OS_PRIORITY = 0;
61
62 /*! Status returned by {@link #getPri} when an error occurs */
63 const Int GETPRI_FAILED = -2;
64
65 /*! Status returned by {@link #compareOsPriorities} when an error occurs */
66 enum CompStatus {
67 CompStatus_ERROR = -2,
68 CompStatus_LOWER = -1,
69 CompStatus_EQUAL = 0,
70 CompStatus_HIGHER = 1
71 };
72
73 /*! Proxy that needs to be bound to an OS specific delegate. */
74 proxy Proxy inherits IThreadSupport;
75
76 /*! Typedef for thread function */
77 typedef Void (*RunFxn)(IArg);
78
79 /*! Struct to hold thread statistics from {@link #stat} */
80 struct Stat {
81 SizeT stackSize;
82 SizeT stackUsed;
83 }
84
85 /*! Assert when timeout passed to {@link #sleep} is zero */
86 config Assert.Id A_zeroTimeout= {
87 msg: "A_zeroTimeout: Timeout value annot be zero"
88 };
89
90 /*! Default thread stack size. */
91 config SizeT defaultStackSize = 0;
92
93 /*!
94 * ======== self ========
95 * Return the currently executing thread's handle
96 *
97 * @param(eb) Pointer to Error.Block
98 * @a(returns) Returns a handle to the currently executing thread.
99 * If the current thread is the main thread, this function
100 * returns `NULL`. NULL is also returned in case of error.
101 */
102 @DirectCall
103 Handle self(Error.Block *eb);
104
105 /*!
106 * ======== start ========
107 * Start threads running
108 *
109 * This function can be used to start all statically created threads,
110 * and all threads created dynamically before this function is called.
111 * Any thread created after this function is called, starts automatically.
112 * (i.e., there is no need to call Thread_start() more than once).
113 *
114 * @param(eb) Pointer to Error.Block
115 * @a(returns) true for success; false for error
116 */
117 Bool start(Error.Block *eb);
118
119 /*!
120 * ======== yield ========
121 * Yield the currently scheduled thread
122 *
123 * @param(eb) Pointer to Error.Block
124 * @a(returns) true for success; false for error
125 */
126 Bool yield(Error.Block *eb);
127
128 /*!
129 * ======== compareOsPriorities ========
130 * Compare two os specific priority values and find out which one
131 * represents a higher priority.
132 *
133 * @p(blist) 134 * -{@link #CompStatus_ERROR} if an error occured
135 * -{@link #CompStatus_LOWER} if p1 is lower than p2
136 * -{@link #CompStatus_EQUAL} if p1=p2
137 * -{@link #CompStatus_HIGHER} if p1 is higher than p2
138 * details.
139 * @p 140 *
141 * @param(p1) priority one
142 * @param(p2) priority two
143 * @param(eb) Pointer to Error.Block
144 * @a(returns) refer to description above
145 */
146 Int compareOsPriorities(Int p1, Int p2, Error.Block *eb);
147
148 /*!
149 * ======== sleep ========
150 * Sleep for given number of microseconds
151 *
152 * This function is gauranteed to sleep for at least as long as the
153 * timeout value but the actual sleep time may be longer. NOTE:
154 * The timeout value cannot be zero.
155 *
156 * @param(timeout) timeout in microseconds
157 * @param(eb) Pointer to Error.Block
158 * @a(returns) true for success; false for error
159 */
160 Bool sleep(UInt timeout, Error.Block *eb);
161
162 instance:
163
164 /*! Thread function argument. Default is 0. */
165 config IArg arg = 0;
166
167 /*!
168 * ======== priority ========
169 * Specify the new thread's priority
170 *
171 * Thread defines several constants which allows applications to select
172 * a priority in an OS independent way: Priority_LOWEST,
173 * Priority_BELOW_NORMAL, Priority_NORMAL, Priority_ABOVE_NORMAL and
174 * Priority_HIGHEST. These values get mapped to OS specific priorities
175 * by the OS specific delegate.
176 */
177 config Priority priority = Priority_NORMAL;
178
179 /*!
180 * ======== osPriority ========
181 * OS specific thread priority
182 *
183 * Used to specify an OS specific value for priority. If set this value
184 * takes precedence over {@link #priority}.
185 */
186 config Int osPriority = INVALID_OS_PRIORITY;
187
188 /*!
189 * ======== stackSize ========
190 * Thread stack size
191 *
192 * The default value of 0 means that `{@link #defaultStackSize}` is used.
193 */
194 config SizeT stackSize = 0;
195
196 /*!
197 * ======== tls ========
198 * Thread local storage.
199 *
200 * User data associated with a thread. Must persist for the life of
201 * the thread.
202 */
203 config Ptr tls = null;
204
205 /*!
206 * ======== create ========
207 * Create a Thread object
208 *
209 * This function spawns a new thread calling the function fxn.
210 *
211 * @param(fxn) function for new thread to begin execution
212 */
213 create(RunFxn fxn);
214
215 /*!
216 * ======== join ========
217 * Block calling thread until given thread terminates.
218 *
219 * Use this functions to ensure that a thread has terminated. It is OK to
220 * call this function on a thread that has already terminated.
221 *
222 * @param(eb) Pointer to Error.Block
223 * @a(returns) true for success; false for error
224 */
225 Bool join(Error.Block *eb);
226
227 /*!
228 * ======== getPriority ========
229 * Obtain a thread's priority.
230 *
231 * For OSes that support dynamic priority boosting, this function
232 * retrieves the base priority of the thread.
233 *
234 * @param(eb) Pointer to Error.Block
235 * @a(returns) thread priority in case of success; PRIORITY_INVALID in
236 * case of error;
237 */
238 Priority getPriority(Error.Block *eb);
239
240 /*!
241 * ======== setPriority ========
242 * Set a thread's priority.
243 *
244 * For OSes that support dynamic priority boosting, this function
245 * changes the base priority of the thread.
246 *
247 * @param(newPri) new thread priority
248 * @param(eb) Pointer to Error.Block
249 * @a(returns) true for success; false for error
250 */
251 Bool setPriority(Priority newPri, Error.Block *eb);
252
253 /*!
254 * ======== getOsPriority ========
255 * Obtain a thread's OS specific priority.
256 *
257 * For OSes that support dynamic priority boosting, the value returned
258 * is the base priority of the thread.
259 *
260 * @param(eb) Pointer to Error.Block
261 * @a(returns) thread priority in case of success; GETPRI_FAILED in
262 * case of error;
263 */
264 Int getOsPriority(Error.Block *eb);
265
266 /*!
267 * ======== setOsPriority ========
268 * Set a thread's priority.
269 *
270 * This API sets the base priority of the thread on OSes that
271 * support dynamic priority boosting
272 *
273 * @param(newPri) new thread priority
274 * @param(eb) Pointer to Error.Block
275 * @a(returns) true for success; false for error
276 */
277 Bool setOsPriority(Int newPri, Error.Block *eb);
278
279 /*!
280 * ======== getOsHandle ========
281 * Get the OS thread handle
282 *
283 * @a(returns) OS thread handle
284 */
285 Ptr getOsHandle();
286
287 /*!
288 * ======== getTls ========
289 * Obtain a thread's local storage.
290 *
291 * @a(returns) null when tls has not been set.
292 */
293 Ptr getTls();
294
295 /*!
296 * ======== setTls ========
297 * Change a thread's local storage.
298 *
299 * @param(tls) tls
300 */
301 Void setTls(Ptr tls);
302
303 /*!
304 * ======== stat ========
305 * Get thread statistics
306 *
307 * @param(buf) Pointer to Stat
308 * @param(eb) Pointer to Error.Block
309 * @a(returns) true for success; false for failure
310 */
311 Bool stat(Stat* buf, Error.Block *eb);
312
313 internal:
314
315 struct Instance_State {
316 Thread.Proxy.Handle proxyHandle; /*! handle for real implementation */
317 Ptr tls; /*! store tls parameter */
318 }
319 }
320
321 /*
322 *! Revision History
323 *! ================
324 *! 17-Apr-2009 nitya Review updates
325 */
326 /*
327 * @(#) xdc.runtime.knl; 1, 0, 0,45; 12-18-2009 12:27:13; /db/ztree/library/trees/xdc/xdc-u16x/src/packages/
328 */
329