1    /*
     2     *  ======== Rta.xdc ========
     3     *
     4     *! Revision History
     5     *! ================
     6     *! 08-Sep-2009 cmcc    Created
     7     */
     8     
     9    package xdc.runtime;
    10    
    11    /*!
    12     *  ======== Rta ========
    13     *  The Rta module contains target and configuration code for providing RTA
    14     *  support.
    15     *
    16     *  The 'Command' enum defines the available control commands, and the
    17     *  'CommandPacket' structure defines the format of commands received from
    18     *  the host. 
    19     *
    20     *  All commands should send back a response, even if only to acknowledge
    21     *  receipt and completion of the command. The format of the response
    22     *  is defined by the 'ResponsePacket' structure.
    23     *
    24     *  The Rta_processCommand can be used to process commands received from a
    25     *  host to call the appropriate API. Alternatively, the individual APIs can
    26     *  be called if not all of the defined commands are used.
    27     */
    28    module Rta {
    29    
    30        /*! Logged when the Agent receives a command */
    31        config Log.Event LD_cmdRcvd = {
    32            mask: Diags.USER2,
    33            msg: "LD_cmdRcvd: Received command: %d, arg0: 0x%x, arg1: 0x%x"
    34        };
    35    
    36        /*! Logged when a diags mask is changed */
    37        config Log.Event LD_writeMask = {
    38            mask: Diags.USER2,
    39            msg: "LD_writeMask: Mask addres: 0x%x, New mask value: 0x%x"
    40        };
    41        
    42        /*! Assert if logger id in control command is invalid. */
    43        config Assert.Id A_invalidLogger = {
    44            msg: "A_invalidLogger: The logger id %d is invalid."
    45        };
    46        
    47        /*! Error raised if Agent receives an invalid command. */
    48        config Error.Id E_badCommand  = {
    49            msg: "E_badCommand: Received invalid command, id: %d."
    50        };
    51    
    52        /*! Command ids */
    53        enum Command : Int {
    54            Command_READ_MASK = 0,  
    55            Command_WRITE_MASK = 1, 
    56            Command_LOGGER_OFF = 2,
    57            Command_LOGGER_ON = 3,
    58            Command_GET_CPU_SPEED = 4,
    59            Command_RESET_LOGGER = 5,
    60            Command_CHANGE_PERIOD = 6
    61        };
    62        
    63        /*! 
    64         * Structure of command received from host 
    65         * TODO - Either the types should be changed to 32-bits, or the packet
    66         * size information should be added to the RTA XML file.
    67         */
    68        struct CommandPacket {
    69            Command  cmdId;
    70            UArg     arg0;
    71            UArg     arg1;
    72        }
    73    
    74        /*! Structure of response packet sent back to host */
    75        struct ResponsePacket {
    76            Command  cmdId;
    77            UArg     resp0;
    78            UArg     resp1;
    79        }
    80        
    81        /*!
    82         *  ======== processCommand ========
    83         *  Executes a command packet and prepares the response packet.
    84         *  
    85         *  This API will execute the command specified by the command packet
    86         *  argument, and will store the response information in the response
    87         *  packet argument.
    88         *
    89         *  @param(cmd)    The CommandPacket to execute.
    90         *  @param(resp)   The ResponsePacket to populate with the response.
    91         */
    92        Void processCommand(CommandPacket *cmd, ResponsePacket *resp);
    93        
    94        /*!
    95         *  ======== acknowledgeCmd ========
    96         */
    97        Void acknowledgeCmd(ResponsePacket *resp);
    98    
    99        /*!
   100         *  ======== readMask ========
   101         */
   102        Void readMask(ResponsePacket *resp, UArg addr);
   103        
   104        /*!
   105         *  ======== writeMask ========
   106         */   
   107        Void writeMask(ResponsePacket *resp, UArg addr, UArg val);
   108        
   109        /*!
   110         *  ======== enableLog ========
   111         */
   112        Void enableLog(ResponsePacket *resp, UArg log);
   113        
   114        /*!
   115         *  ======== disableLog ========
   116         */
   117        Void disableLog(ResponsePacket *resp, UArg log);
   118        
   119        /*!
   120         *  ======== getCpuSpeed ========
   121         */
   122        Void getCpuSpeed(ResponsePacket *resp);
   123        
   124        /*!
   125         *  ======== resetLog ========
   126         */
   127        Void resetLog(ResponsePacket *resp, UArg log);
   128        
   129        /*!
   130         *  ======== changePeriod ========
   131         */
   132        Void changePeriod(ResponsePacket *resp, UArg period);
   133    
   134        /*!
   135         *  @_nodoc
   136         *  ======== genRta ========
   137         *  Generates the Rta XML file.
   138         */
   139        function genRta(outputFileName);
   140    
   141    }
   142    /*
   143     *  @(#) xdc.runtime; 2, 0, 0, 0,236; 12-18-2009 12:27:14; /db/ztree/library/trees/xdc/xdc-u16x/src/packages/
   144     */
   145