From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 02-Oct-2009 22:10 UTC | ![]() |
XDCspec - @Facet
This meta-only unit or config parameter is a facet
The @Facet attribute can only be applied to meta-only modules, interfaces, or Instance config parameters.
A module can have any number of Facet config parameters, but a module may not contain more then one Facet config parameter of the same type.
A Facet config parameter can only reference Instances of modules that are themselves declared to be Facets.
Using a module's or interface's $spec property, it is possible to "query" a module in the meta-domain to determine if it has a particular facet.
| var SysMin= xdc.module("xdc.runtime.SysMin"); /* get the name of the "xdc.rov.ViewInfo" fact config parameter */ var facet = SysMin.$spec.queryFacet("xdc.rov.ViewInfo"); if (facet != null) { /* if SysMin has the "xdc.rov.ViewInfo" facet, get the instance */ var inst = SysMin[facet]; : } |
See also
XDCscript - Module-Object.$spec | Module specification object |
xdc.services.spec | Client documentation for xdc.services.spec |
![]() | [printable version] [offline version] | offline version generated on 02-Oct-2009 22:10 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved