From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 02-Oct-2009 22:10 UTC | ![]() ![]() |
Demo of RTSC Project Creation in CCSv4
Using CCStudio v4 to create a RTSC project
This Flash demo shows how to create a CCSv4 project that has RTSC support enabled. In this example, a DSP/BIOS "hello world" template is used when creating the project.
When the demo pauses, click "Next" to continue. A table of contents at the end lets you review specific actions.
If you don't see the demo, you can download the Flash player, or save the demo to disk.
See also
RTSC+CCStudio v4 QuickStart | Using CCStudio v4 to create, build, and debug RTSC projects |
RTSC+Eclipse FAQs | Using RTSC with Eclipse-Based Tools |
XGCONF User's Guide | Using the RTSC Graphical Configuration Tool in CCSv4 |
Runtime Object Viewer | Using ROV for Eclipse-Based Debugging |
![]() | [printable version] [offline version] | offline version generated on 02-Oct-2009 22:10 UTC | ![]() ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved