From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 02-Oct-2009 22:10 UTC | ![]() |
C - Object get
Get the instance handle of a statically created instance
Contents |
Synopsis
| #include <«pkg»/«Mod».h> «Mod»_Handle «Mod»_Object_get(«Mod»_Object *array, Int index); |
Description
This function is automatically defined for all target modules, where «Mod» is the name of some module. This function is typically used in situations where the «Mod» needs to loop over all statically created instances. If the first argument is NULL, «Mod»_Object_get() loops over the statically created instances created by «Mod».
| for (i = 0; i < «Mod»_Object_count(); i++) { «Mod»_Handle h = «Mod»_Object_get(NULL, i); : /* use «Mod» instance referenced by h */ } |
Dynamically created instances are not returned by «Mod»_Object_get() and must be accessed via «Mod»_Object_first() and «Mod»_Object_next().
See also
C - Object_count | Get the number of statically created instances |
C - Object_first | Get the handle of the first dynamically created instance |
C - Object_next | Get the handle of the next dynamically created instance |
![]() | [printable version] [offline version] | offline version generated on 02-Oct-2009 22:10 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved