1 /*
2 * Copyright (c) 2008 Texas Instruments and others.
3 * All rights reserved. This program and the accompanying materials
4 * are made available under the terms of the Eclipse Public License v1.0
5 * which accompanies this distribution, and is available at
6 * http://www.eclipse.org/legal/epl-v10.html
7 *
8 * Contributors:
9 * Texas Instruments - initial implementation
10 *
11 * */
12 /*
13 * ======== ITarget.xdc ========
14 */
15 package microsoft.targets;
16
17 /*!
18 * ======== ITarget ========
19 * A Microsoft-specific extension to the base xdc.bld.ITarget interface.
20 */
21 @TargetHeader("xdc/bld/stddefs.xdt")
22 metaonlyinterface ITarget inherits xdc.bld.ITarget {
23
24 overridereadonlyconfig string stdInclude = "microsoft/targets/std.h";
25 overrideconfig string dllExt = ".dll";
26
27 /*!
28 * ======== debugGen ========
29 * Debugger/IDE project file generation support.
30 *
31 * The settings below generate VC project files that enable one
32 * to debug (and even rebuild) Executables from within the VC GUI.
33 *
34 * To avoid unnecessary build time overhead, these files are not always
35 * generated; by default, they are only generated for "debug" profiles.
36 * The generation of these files is controlled by the
37 * `{@link xdc.cfg.Program#gen}` configuration parameter. To force these
38 * files to be generated for a particular executable, add the following
39 * line to the executable's program configuration script:
40 * @p(code) 41 * Program.gen.debuggerFiles = true;
42 * @p 43 * It is also possible to control the generation via build options; see
44 * `{@link xdc.bld.ITarget#DebugGen}`.
45 *
46 * To debug an executable: double click on the generated *.vcproj file,
47 * when the debugger comes up, type F11 (step into).
48 *
49 * The first time you debug an executable, the VC debugger may prompt
50 * you for a "solution file" to save. Click OK (accepting the solution
51 * file name), and you will be at the first statement of your
52 * executable.
53 *
54 * To set command line arguments prior to debugging: open the
55 * executable's "Project Properties" dialog (select the
56 * executable in the "Solution Explorer" window and pull-down
57 * View->"Property Pages" or type shift-F4), select "Debugging"
58 * in the left-most pane of the executable's "Property Pages", and
59 * enter command line arguments in the "Command Arguments" text box.
60 *
61 * @see http://msdn.microsoft.com/library/default.asp?url=/library/en-us/vsdebug/html/vxtskdebugginganexecreatedwithoutvisualstudioproject.asp
62 */
63 overrideconfig xdc.bld.ITarget.DebugGen debugGen = {
64 execTemplate: "microsoft/targets/vc_exec.xdt",
65 execPattern: "$(cfgName).vcproj"
66 };
67
68 /*!
69 * ======== profiles ========
70 * Standard options profiles for the microsoft tool-chain.
71 */
72 overrideconfig xdc.bld.ITarget.OptionSet profiles[string] = [
73 ["debug", {
74 compileOpts: {
75 copts: "-Z7 -Odi -MTd",
76 defs: "-D_DEBUG=1",
77 },
78 linkOpts: "-debug msvcrt.lib setargv.obj oldnames.lib ole32.lib oleaut32.lib olepro32.lib uuid.lib kernel32.lib user32.lib gdi32.lib advapi32.lib shell32.lib comctl32.lib",
79 }],
80
81 ["release", {
82 compileOpts: {
83 copts: "-O2 -MT",
84 defs: "",
85 },
86 linkOpts: "msvcrt.lib setargv.obj oldnames.lib ole32.lib oleaut32.lib olepro32.lib uuid.lib kernel32.lib user32.lib gdi32.lib advapi32.lib shell32.lib comctl32.lib",
87 }],
88 ];
89
90 /*!
91 * ======== Command ========
92 * Required command and options.
93 *
94 * The compile, link, and archive functions in this interface are
95 * implemented by expanding the strings specified in this structure
96 * and inserting strings from the Options structure to form a single
97 * command. The strings in this structure can not be changed by
98 * the user (they are fixed by the target), but the string in the
99 * Options structure may be changed by the user.
100 *
101 * The final command is:
102 * Command.cmd Options.prefix Command.opts Options.suffix
103 *
104 * @field(cmd) name of a tool-chain executable without any path
105 * information. The location of this executable is
106 * specified by the binDir (or pathPrefix)
107 * configuration parameter.
108 *
109 * @field(opts) required options passed to the command; these options
110 * can not be changed or eliminated by user's
111 * configuration script.
112 */
113 struct Command {
114 string cmd; /*! the command to run */
115 string opts; /*! required options for the command */
116 }
117
118 /*!
119 * ======== Options ========
120 * User configurable command options.
121 *
122 * The option strings allow the user to pass additional parameters to the
123 * executable that is responsible for compiling, linker, or archiving.
124 *
125 * @a(see) 126 * microsoft.targets.ITarget.Command
127 */
128 struct Options {
129 string prefix; //! options placed before required command options
130 string suffix; //! options placed after required command options
131 }
132
133 /*!
134 * ======== ar ========
135 * The command used to create an archive (i.e., library)
136 */
137 readonlyconfig Command ar;
138
139 /*!
140 * ======== arOpts ========
141 * User configurable archiver options.
142 */
143 config Options arOpts = {
144 prefix: "",
145 suffix: ""
146 };
147
148 /*!
149 * ======== lnk ========
150 * The command used to link executables.
151 */
152 readonlyconfig Command lnk;
153
154 /*!
155 * ======== lnkOpts ========
156 * User configurable linker options.
157 */
158 config Options lnkOpts = {
159 prefix: "",
160 suffix: ""
161 };
162
163 /*!
164 * ======== cc ========
165 * The command used to compile C/C++ source files into object files
166 */
167 readonlyconfig Command cc;
168
169 /*!
170 * ======== ccOpts ========
171 * User configurable compiler options.
172 */
173 config Options ccOpts = {
174 prefix: "",
175 suffix: ""
176 };
177
178 /*!
179 * ======== asm ========
180 * The command used to assembles assembly source files into object files
181 */
182 readonlyconfig Command asm;
183
184 /*!
185 * ======== setPath ========
186 * Return path needed to find necessary DLLS
187 *
188 * The microsoft compilers often require one or more directories to
189 * be in the PATH; this allows the compiler to find necessary DLLs.
190 * A target implementing this function returns a string with path
191 * components separated by ";".
192 */
193 function setPath();
194
195 /*!
196 * ======== cmdPrefix ========
197 * Prefix to put in front of each command
198 *
199 * This string is put in front of every Command before being passed to
200 * the shell for execution. This string can be used to run the compiler
201 * in emulation environments.
202 */
203 config String cmdPrefix = "";
204
205 /*!
206 * ======== strictANSI ========
207 * Disable Microsoft C/C++ language extensions
208 *
209 * Set to true if you plan to port your program to other environments.
210 * The compiler treats extended keywords as simple identifiers, disables
211 * the other Microsoft extensions, and automatically defines the
212 * `__STDC__` predefined macro for C programs. This option shows up
213 * as `"-Za"` on the command line when strictANSI is set to `true`.
214 */
215 configbool strictANSI = true;
216
217 /*!
218 * ======== version ========
219 * The Compatibility Key associated with this target.
220 *
221 * The first two components of this target Compatibility Key are '1,0'.
222 * The rest of the Key represents the compiler version. The third
223 * component combines the major and the minor version number in the format
224 * Major.Minor. The fourth component is the build number.
225 *
226 * @a(Example) 227 * If this target's `rootDir` points to the Visual C++ 2005 Express
228 * Edition, the output of the command `cl` may contains the compiler
229 * version string 14.00.50727.42. The Compatibility Key is
230 * [1,0,14.00,50727].
231 *
232 */
233 overridemetaonlyconfig String version;
234
235 /*!
236 * ======== asmOpts ========
237 * User configurable assembler options.
238 */
239 config Options asmOpts = {
240 prefix: "",
241 suffix: ""
242 };
243
244 /*!
245 * ======== includeOpts ========
246 * Additional user configurable target-specific include path options
247 */
248 config string includeOpts;
249
250 /*!
251 * ======== stdTypes ========
252 * @_nodoc 253 */
254 overridereadonlyconfig xdc.bld.ITarget.StdTypes stdTypes = {
255 t_IArg : { size: 4, align: 1 },
256 t_Char : { size: 1, align: 1 },
257 t_Double : { size: 8, align: 1 },
258 t_Float : { size: 4, align: 1 },
259 t_Fxn : { size: 4, align: 1 },
260 t_Int : { size: 4, align: 1 },
261 t_Int8 : { size: 1, align: 1 },
262 t_Int16 : { size: 2, align: 1 },
263 t_Int32 : { size: 4, align: 1 },
264 t_Int64 : { size: 8, align: 1 },
265 t_Long : { size: 4, align: 1 },
266 t_LDouble : { size: 8, align: 1 },
267 t_Ptr : { size: 4, align: 1 },
268 t_Short : { size: 2, align: 1 },
269 };
270 }
271 /*
272 * @(#) microsoft.targets; 1, 0, 2, 0,370; 11-25-2009 10:23:05; /db/atree/library/trees/xdctargets/xdctargets-b28x/src/
273 */
274