From RTSC-Pedia
revision tip
LANDSCAPE orientation[printable version] [offline version] | offline version generated on 02-Oct-2009 22:10 UTC |
XDCspec - @Encoded
This type has custom encoding
Types with the Encoded attribute have runtime representations that differ so significantly from the meta-domain representation that the default C representation of these types must be overridden. The runtime representation is explicitly defined by the module producer by:
- declaring the C type in the module's (normally optional) custom C header files, and
- defining conversions from the meta-domain objects of an encoded type to a runtime value in the module's (normally optional) meta-domain implementation file.
For more details about encoded types, see Using Encoded Types.
[printable version] [offline version] | offline version generated on 02-Oct-2009 22:10 UTC |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved