1 /* --COPYRIGHT--,ESD
2 * Copyright (c) 2008 Texas Instruments. All rights reserved.
3 * This program and the accompanying materials are made available under the
4 * terms of the Eclipse Public License v1.0 and Eclipse Distribution License
5 * v. 1.0 which accompanies this distribution. The Eclipse Public License is
6 * available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
7 * Distribution License is available at
8 * http://www.eclipse.org/org/documents/edl-v10.php.
9 *
10 * Contributors:
11 * Texas Instruments - initial implementation
12 * --/COPYRIGHT--*/
13 /*
14 * ======== Timestamp.xdc ========
15 *
16 *! Revision History
17 *! ================
18 *! 11-Mar-2008 agd xdc runtime review changes
19 *! 14-Dec-2007 sasa started revision history
20 */
21
22 package xdc.runtime;
23
24 /*!
25 * ======== Timestamp ========
26 * Timestamp services
27 *
28 * This module provides `{@link xdc.runtime.ITimestampClient}` APIs for
29 * the xdc Runtime Support Library. Calls to these APIs are forwarded
30 * to a platform specific `{@link xdc.runtime.ITimestampProvider}`
31 * implementation.
32 *
33 * A user can attach their own ITimestampProvider module
34 * using the following config file command:
35 * @p(code) 36 *
37 * xdc.runtime.Timestamp.SupportProxy = xdc.useModule("usersTimestampProvider");
38 * @p 39 * If no such `{@link #SupportProxy SupportProxy}` initialization is done,
40 * the `{@link xdc.runtime.TimestampNull}` ITimestampProvider implementation,
41 * which provides null stubs for the APIs, will be attached by default.
42 *
43 * If the user is developing code using CCS, the
44 * `{@link xdc.runtime.TimestampStd}`
45 * ITimestampProvider implementation, which uses the ANSI C clock()
46 * function, may provide a satisfactory timestamp source (remember to
47 * enable the profile clock in CCS).
48 *
49 * To use the TimestampStd implementation, add the following to
50 * your config script:
51 * @p(code) 52 *
53 * xdc.runtime.Timestamp.SupportProxy = xdc.useModule("xdc.runtime.TimestampStd");
54 * @p 55 */
56 module Timestamp inherits ITimestampClient {
57
58 /*!
59 * ======== SupportProxy ========
60 * User supplied time stamp provider module.
61 *
62 * The SupportProxy module provides application/platform
63 * specific implementations of the
64 * `{@link xdc.runtime.ITimestampProvider}` APIs.
65 *
66 * If not explicitly supplied by the user, this proxy defaults to
67 * `{@link xdc.runtime.TimestampNull}`,
68 * which provides null stubs for all of the ITimestampProvider APIs.
69 */
70 proxy SupportProxy inherits ITimestampProvider;
71 }
72 /*
73 * @(#) xdc.runtime; 2, 0, 0, 0,231; 10-7-2009 16:21:31; /db/ztree/library/trees/xdc-u12x/src/packages/
74 */
75