From RTSC-Pedia
revision tip
LANDSCAPE orientation[printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC |
XDCspec - @Facet
This meta-only unit is a facet
The @Facet attribute can only be applied to meta-only modules, interfaces, or Instance config parameters.
A module can have any number of Facet config parameters, but a module may not contain more then one Facet config parameter of the same type.
A Facet config parameter can only reference Instances of modules that are themselves declared to be Facets.
[printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved