From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC | ![]() |
XDCscript - xdc.om.$name
Model name
Contents |
Synopsis
| var name = xdc.om.$name; |
Description
Each domain object model has a name that can be used by scripts that need to run in multiple models. The name of the current object model can be accessed via the $name property of xdc.om; i.e., xdc.om.$name. The current model names include the following:
- "bld" - build model
- "cfg" - configuration model
- "rov" - runtime object view model
Example
This property is often used within package methods for packages that are loaded and used in more than one model. For example, a package that is can be used in both the build model and the configuration model might have the following close() implementation.
| function close() { if (xdc.on.$name == "cfg") { /* Program is defined by the config model but not the build model */ if (Program.stackSize < 512) { : } } } |
![]() | [printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved