From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC | ![]() |
XDCscript - xdc.getWarnings
Return array of warnings
Contents |
Synopsis
| var warnings = xdc.getWarnings(); |
Description
Each module can raise an warning that does not terminate processing of a domain model's "validate" phase, for example. xdc.getWarnings() returns the current array of warnings raised by modules.
Return Value
xdc.getWarnings() returns a non-null array of warnings raised modules via their $logWarning() method.
Since
This method was introduced in XDCtools release 3.15.
![]() | [printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved