From RTSC-Pedia
revision tip
LANDSCAPE orientation[printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC |
XDCscript - xdc.getErrors
Return array of errors
Contents |
Synopsis
| var errors = xdc.getErrors(); |
Description
Each module can raise an error that does not immediately terminate processing of a domain model's "validate" phase, for example. xdc.getErrors() returns the current array of errors raised by modules.
Return Value
xdc.getErrors() returns a non-null array of errors raised modules via their $logError() method.
Since
This method was introduced in XDCtools release 3.15.
[printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved