From RTSC-Pedia

Jump to: navigation, search
revision tip
—— LANDSCAPE orientation
[printable version]  [offline version]offline version generated on 11-Jun-2009 18:06 UTC

XDCscript - Typed-Object.$seal

Seal a typed object or one of its fields

Contents

Synopsis

 
«tobj».$seal(«fieldName»)

Description

Renders the specified field within «tobj» read-only. If «fieldName» is omitted, the entire object is made read-only.

See also

XDCscript - Typed-Object Objects specified by the RTSC Interface Definition Language
XDCscript - Typed-Object.$sealed Test a typed object or one of its fields for being read-only
XDCscript - Typed-Object.$unseal Unseal a typed object or one of its fields

[printable version]  [offline version]offline version generated on 11-Jun-2009 18:06 UTC
Copyright © 2008 The Eclipse Foundation. All Rights Reserved


Views
Personal tools
package reference