From RTSC-Pedia
revision tip
LANDSCAPE orientation[printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC |
XDCscript - Template-Object.genFile
Generate textual output file from a template
Contents |
Synopsis
| var tplt = xdc.loadTemplate(templateFile); tplt.genFile(outputFile, thisObj, args, clobber); |
Parameters
- outputFile
- string name of the output file to be created
- thisObj
- object that is referenced within the template via this
- args
- array of arguments referenced within the template via $args
- clobber
- boolean which, if true, causes genFile to overwrite outputFile even if the contents of an existing file are identical to the template output
Description
Generates output to a specified file, which is created if necessary. Unless clobber is true, an existing file is overwritten only when its content has truly changed. Internally calls genStream().
See also
XDCscript - Template-Body | Contents of the template file |
XDCscript - Template-Object.genStream | Generate textual output stream from a template |
[printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved