From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC | ![]() |
XDCscript - Module-Object.$instances
An array of instance objects managed by this module
Contents |
Synopsis
| «Mod».$instances |
where «Mod» is a module object.
Description
The $instances property of a module object is an array of all Instance objects that have been created (via «Mod».create()) during configuration. This array does not contain any embedded instances. To get the list of all instance that are embedded in other objects, you can use «Mod».$objects.
Example
| var LoggerBuf = xdc.module("xdc.runtime.LoggerBuf"); for (var i = o; i < LoggerBuf.$instances.length; i++) { print(LoggerBuf.$instances[i]); } |
See also
XDCscript - Module-Object.create | Create a new Instance object managed by this unit |
XDCscript - Module-Object.$objects | An array of embedded instance objects managed by this module |
![]() | [printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved