From RTSC-Pedia
revision tip
LANDSCAPE orientation[printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC |
XDCscript - Instance-Object.$package
The Package object containing the module managing this instance
Contents |
Synopsis
| «inst».$package |
Description
The $package property of an instance object is the Package object which contains the module that manages this instance.
See also
XDCscript - Instance-Object.$module | The Module object that manages this instance |
[printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved