From RTSC-Pedia
revision tip
LANDSCAPE orientation![]() | [printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC | ![]() |
C - Module id
Get a module's unique ID
Contents |
Synopsis
| #include <«pkg»/«Mod».h> #include <xdc/runtime/Types.h> Types_ModuleId «Mod»_Module_id(void); |
Description
This function is automatically defined for all target modules, where «Mod» is the name of some module. This function returns the configuration generated module ID for «Mod». This ID is used to identify the source of raised errors, for example. For more information see xdc.runtime.Types_ModuleId.
See also
xdc.runtime.Types.ModuleId | Client documentation for xdc.runtime.Types.ModuleId |
![]() | [printable version] [offline version] | offline version generated on 11-Jun-2009 18:06 UTC | ![]() |
Copyright © 2008 The Eclipse Foundation. All Rights Reserved